Category: Hardware
Product Number: ADF4382A , ADF4382
将ADF4382A加电后,参考输入是100MHz,我想输出12.5GHz的信号。MAX_OUT可以是正常输出,锁定指示为低,请问Div_Nclk/2和Div_Rclk/2指的是什么?我的VCO完全没有任何信号输出,这是为什么?下面是我的寄存器。
unsigned int ADF4382A[57] = {
0x005345、0x005000、0x004D00、0x004B5D、0x004552、0x00442E、
0x004201、0x004100、0x004000、0x003F82、0x003E3E、0x003D20、
0x003C00、0x003B00、0x003AFA、0x003900、0x00387C、0x0037CA、
0x003680、0x00353F、0x003436、0x003300、0x003240、0x00316B、
0x00302F、0x002FFF、0x002E10、0x002DF1、0x002C09、0x002B00、
0x002A20、0x002909、0x002800、0x0027F0、0x002600、0x002501、
0x002400、0x002300、0x002200、0x002100、0x002081、0x001F17、
0x001E28、0x001DFB、0x001C00、0x001B00、0x001A01、0x001900、
0x001800、0x001700、0x001685、0x001582、0x001400、0x001300、
0x001200、0x001110 0x00107D
};