Post Go back to editing

DC2222A-B(LTC2508)及DC890B在使用时时钟报错,没能正常采集数据。

Category: Hardware
Product Number: LTC2508-32
1.pscope软件正常检测到DC222A-B与DC890B,按下图设置参数且其他参数均为默认参数的情况下启动collect,两个板子仿佛没有正常工作,软件显示“时钟错误,请检查时钟源或正确配置时钟速率”,多次尝试采集都显示该报错。更换电脑再次尝试报错为“DATA COLLECTION TIMEOUT”
 
2.使用逻辑分析仪测量时钟信号,发现,在采集前,ADC有时钟信号,开始采集后U3触发器输出的信号消失, ,且停止采集后时钟依然不回复,除非断电再重新上电。
 
3.在不使用DC890B与PScope软件,仅使用单片机通过杜邦线连接DC2222A-B控制ADC采集并收集SPI的数据时,发现ADC能正常工作并采集到数据。
 
4.下图是上面“1.”的试验时某一次偶然测到的数据(并没有给信号源),这样偶然测到数据的情况一共有两次。

Thread Notes

Parents
  • 楼主,请问有解决方法吗?我在使用DC2222A-A(LTC2500-32)和DC890B时遇到了相同的问题:“时钟错误,请检查时钟源或正确配置时钟速率”,“DATA COLLECTION TIMEOUT”

Reply
  • 楼主,请问有解决方法吗?我在使用DC2222A-A(LTC2500-32)和DC890B时遇到了相同的问题:“时钟错误,请检查时钟源或正确配置时钟速率”,“DATA COLLECTION TIMEOUT”

Children
No Data