Post Go back to editing

LT3750高压电容充电电路工作异常

Category: Hardware
Product Number: LT3750

我使用LT3750控制器设计了一个高压电容充电电路。测试发现栅极驱动输出占空比不到10%,充电电流太小,无法将电容电压充电到预设值。设计如下图


Rout=60.4K

RBG=2.49K
RDCM=43K

变压器初次级匝数比1:50  

变压器初级绕组电感量10uH

此电路配置在测试时发现,电路无法启动充电

将RDCM改为220K后,能充电但充电电流太小,充电速度慢,无法将电容充到1500V,实际只能充到500V左右。

备注:我使用LTSPICE仿真过这个电路,仿真发现只要将检测电流的电阻从25mΩ改为15mΩ以下的值,就能运行充电,但是按照仿真实际搭建电路后发现无法运行!

希望能联系到相关的工程师解决这个问题!

我的邮件地址1974478446@qq.com

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.