Post Go back to editing

ad4932

Category: Hardware
  • 我使用adc driver tool 对AD4932-1+LTC2387-18进行仿真。仿真参数如图1所示。当我设置+Vs为5V时,仿真工具提示运放输出4.1V时正电的裕量不够,当我设置-Vs为-1V时,仿真工具提示当Vin=0时,-Vs的裕量不够,当我增大+Vs减小-Vs时,仿真工具不再报红。但是当我用LTspice进行仿真时,设置+Vs=6V –V=-1.9V,运放的vom=2.048v 单端输入摆幅为4 、Vcm_in=0的正弦波,为什么运放可以正常输出波形,仿真设置及仿真波形如下所示。在这种情况下,运放输入了最高可达-4V的负电,而-Vs只有-1.9V,按照我的理解,负电的裕量应该更不够啊,但是输出波形为什么是正常的,这好像和adc driver tool 矛盾。请问是我哪里理解错了,所以,当我设置+Vs=6V,-Vs=-1.9V, Vcom=2.048V AD4932是否可以将单端输入摆幅为4 、Vcm_in=0的正弦波转换为差分信号呢

Thread Notes

Parents Reply Children
No Data