Post Go back to editing

ADV7513内部是否包含YUV422转RGB888(RGB444)

Category: Software
Product Number: ADV7513
Software Version: ISE14.7

Hi,您好

我在使用ADV7513的过程中,一直使用YUV422的输入模式,硬件工程是也只预留16个管教,只能使用内同步YUV422模式,作为视频输入信号,HDMI输出也是YUV422输出的,现在我想采用YUV422的视频输入,HDMI输出是RGB888(RGB444)的格式。

请问:

          1、芯片知否支持内部同步YUV422(BT1120)转RGB444(我在芯片手册中看到寄存器地址,0x17[2]有这个功能,但是不明白他说的含义。zero order和first order)

          2、能否发送我一份初始化配置表,功能是YUV422(8bit)视频输入,RGB888(RGB444)HDMI视频输出,视频格式为1080P 50帧

Hi, Hello!

In the process of using ADV7513, I have been using YUV422 input mode, and the hardware engineering only reserves 16 disciplines. I can only use the internally synchronized YUV422 mode as the video input signal, and the HDMI output is also YUV422 output. Now I want to use YUV422 video input, and the HDMI output is in RGB888 (RGB444) format.

Excuse me?

1. Does the chip support internal synchronization of YUV422 (BT1120) to RGB444? (I saw in the datasheet that the register address 0x17 [2] , but I don't understand what it means.zero order or first order)

2. Can you send me an initialization configuration table with YUV422 (8-bit) video input, RGB888 (RGB444) HDMI video output, and a video format of 1080P 50 frames per second


笔记

Thread Notes