Post Go back to editing

ZCU102+AD9986评估

Category: Software
Product Number: AD9986

Hi:

想请教一下ZCU102+AD9986 demo板评估事宜,只用到AD9986的ADC模块,测试其性能:

1、根据网站wiki.analog.com/.../zynqmp  下载image、systemdtb和boot.bin,将文件拷贝在SD卡里。用于启动102板子和加载AD9986评估板;

2、参考网站的操作流程,ZCU102和评估板可以正常起来,通过串口可以获取设备信息、状态,下载IIO软件可以进行频谱仿真,打开软件后发现ADC的采样频率为3GHz,FFT宽度为1.5GHz,但是我们想评估ADC带宽2.4GHz的性能,ADC的配置为实数输入,采样6GHz,复数输出,使能Coarse DDC,抽取为2,旁路掉Fine DDC;

3、查看设备树的配置,ADC的采样率为6GHz,但是内部抽取为4,是否可以通过更改设备树的来满足我的测试需求,附件为原设备树文件,还有我修改设备树的文档,请帮忙看看是否正确;

b#e�
E-SafeNetLOCK��OB�C,�gWn�m�����ڷbI=a�(�^#����?��B��q�V:�%i�vr��K����g�T��ҟ����y��h�� j"�L)�����|�� LD���!Kԋyχ�AuTM/�-�X:�G�ͣX�o�G#=+�s>}+���V����=�y��OJ3�j\�jU�9t�O2��mG��f�٩���ue��ÓKD4r�S�	��G��D�������6���{cJi=(@w�@��l���q���ъ�������KNA�ņ�z���W>��G��g��������=}=f�4�5�����A���*�-+�:#����^��S1�Y�������?�p�+�ل'O�hF����z��cAR����,��$ݗ�/uu�T+���AX�X�ͤ\�b�i�=3`,���"]����#���O%B�^Z��w�QL�L[��+��ة7��b���r-dYx�^�O����D����w��j�C�e�W3(
3!D�����w女����|������k-+����3���<��W��j��Q��4h	O��F���bFD���l�a�� ��٣�i�@u�#����OF�
o����P�\=R�gby������Ϻ�
��<:�C�{��,��/���g �����%������|a��C�ݹ�0ρD�˒GQɆ�Q��%�����=���vnx-��/MlX�A�s��R�B�xm�<�I3V��\Y�Y�9Fk;+��J���C≩S7�B�c�s�-�����D'rW?^���d6�àȪ����kBy|9�|�0�����A��D|�|@}�I9�y�0�b����uR��4߂߃���M�s���ڀx/�b��ᣮ2��1F����q��E����/Gي�CY�F��_��	�>�	yDI�O
>W��v�E?_���S�0��*@8��{�G�xm��+��dҮ~��<O�k��		5�O�R����F����M���x�\�A?|bJl�M���e������J������(&K҄��z���(����`�6�A@E܈\��#K����/�6ޒc��;���A0�d�x���#o�#Z�p՗�u�0-	{�^*���sߥ���pü�1�C�%�F��HŪ�.K.w�Ƴ|an���[(�����FY��G�ݹ�]��)�ΗFYŋ�
��z������rmxE�z*�IB~T�R�h����d0�e�a��e(�d�c/L��n���V���S
��r�6�q[��A���osY:h���d6���ܫΝ��c7qu�v�K{����m��-��_M�
{D�{I�}�0�b��	��6V��"�������Y�����
7v�P�������-7����c��a�ҵ�-N����R��\��3��>K@J�!j=x��h�Gy}���)�K�B$A�Z��w�_G�}[��+����>��7J�i��V@&��O��C��J����t��j�C��~!<?�����9���������z��u*tbΐ��-���6M��nɻ�y�0��ULVH��K���#K������c�?�욉,P�K�����}B�l�ą�X�s�|-����6�潾�
�R_�9��|�no��c���<4+���>x7��!�n���_��?p��l������Gܦ�[؀�E��g��_�N��0���TE��/%a_�C�h���^� i�t�Bl��ap�(�l9O��n������*U��q�+[� ��L���To:V1U��+�g6���ԭ����o!/%�$�Tk����t��8ԔS�xC}�Ig�~l�J�F����yݐ`�އ����?�pśy���Nn*�o�����"��6)4����n��a�تC�}���X�
��P����>K*/�&hD~*��*�g?Ŕ��y�A��yI�DդJ�f~�.;��9��;�k��[��qX�}��W@3�H�R����E����t��j�9��z #Yq�M���lԟ�������%��|f:b��ŭ#���2N��n���`�,��Q\HI@��G���$���������٣�i�K�����6&�n�%���O
�WGyR�w&{����2�����
�8Z�:�@�*�o*��"���E&NR���j{e���}����p`Ջ|�ゥ0ρD�ʈ��H�I��/��]�O��i�Ńvnx-�g�ObT�B�*����s,�~�:�$%�>�!jme��[��W���G!h�"��z
�<F��M��6,Jgטe�\��ژ�����9Wwl5�4�v����/ɥh��OA�E1D�~�~�0�����6��5��Ӄ����E֐'��;v�ZB�����s��!TR��ޑnܐ.�٣U�5ƒ���Z��4��>K('�is[2%��o�[!k؊��(�\��Zi�_JA��#�Z�vh��+��	��+��7_�m��V@4�_���������F��j�C�
�Z\o9#aB����8�������L���8��+CK+�ᔱz޿�T-��J���u�u��Y\HI��\���:(����v�k��d��P����Wt�i�3����>�=]���7�Po�>tf����c����fü�1�G�%�F��H���cH72���a|s��_�Z8ܴ���|(��n������}��f?��l�Q��f��B�C��y���DL�#~�8I��*��_�N�0e�7�x7U��6<�3�uMwc5��J���W���[r��#�D�d�����Dkv8n��L�R���������<>t4h�3�:����,�� ڛHA�A�4p�Drs��_ڡ�ld��=�ن�ߌ�C�O��x���?r�:�����=
����9'��!̀�K#�(V���HQ���V��L�?�kr!.�r3jH��n�/����i�
��V=�?JQ��p�[C�)#��:܈�do��:��6U�9��Ga�O6�b��2���ٴ�صS�1�f�:yE5l�A���i������x����m��ud-'Fӆ��v�����"��+�O���0ku|`,(�����eZE����?�8��nT��8�욉,8�!�a���k"�g�5ę�FH�
x�^Bꡠ���Ϻ�`��_^�%�@�e�F��H���(z{���?:?��&�n鍌Z��)(�� ��ԎW��(���Iq�:�u�����*ʩ���
]@�eo�C^(��b�Q�s�	\��Z5��'9�5�uOms ��G������=sl�"�,�c�?�����:.'2E���d6���ݥ��ڢ>to;�	�/����{��-ό�-Y�!)�T'>�}�=��9ɩ~ߗ]����ڧR�U��f���_+{�]�����)��-7�ޒ�hW��%�ҵ�8���D���o��0��V& o� pSl'��i�X&z����8���*@8�A4ңM�f~�%>�gG��=�k��[��[K�~��[](A�J�e��2��������
�/�A�RzlUp[j�8�ݛ����˦��x��ҝl�tc?+F����3��'��jʻn��9��@S���ˏ.����!��c��	�,P�yn�r���w�xk���7
�^=R�gb{������Ϻ�b��U�=��{�&!��$잖mi���JNB���\��7��-4ė*����\��p�����^�:��C�L�I�����	IK�v&�8I��!��f�w�}n��x7U��68�>�=NB&u��j���;��U:X��o�zP�<��u��6nyׇt�	���������A0F�O�tV����=˜B��vx�-�$-�~{��K����g�Y��䊷����u���Bo#�\o�����,��-7�ގ�q��E���A�3Gƹ��'��k��0�k�i�=3T`,���"]���<�M��G,U�
T��z�M1�ٰLd��@�O]��[��[0�}��M9��O��C��J����t��j�.�@�Ai)}#A�]��/��˦��x������@K+����}���w��jʻn��*��\\IY]��Pɤ�:(�3�p��c������d�RK�T��َ�ED�7q�X@i^�>l"��߇;���˚3ӿ
=�@�{��o&�3���=*4���2(=���Y#��7��E1��b������`�ֈP���Q��G�$�)�����rJ)��

1882.设备树修改.docx

Thread Notes

Parents Reply Children
No Data