Post Go back to editing

Can I use the CN0510(EVAL-AD5941BATZ) to measure human body impedance?

Category: Hardware
Product Number: CN0510

My english is very poor.So I will use translation software to express my question.

I want to use CN0510 to  measure  Body Impedance(BIA) and Skin impedance.But I don't konw what to use the BNC connect  body. 重试    错误原因

I know that EVAL-AD5941BATZ is specially used to measure batteries. I bought the wrong model at the beginning, and now I want to use the existing board for measurement.

I saw in the manual that the AD594x series supports the measurement of body impedance and skin impedance, so I want to know if the 5941BATZ I currently have can measure body impedance. 重试    错误原因

The above is the current status of my wiring and data output. Seeing this status, I don't know how to correct it to display normal values. Perhaps it's a problem with the code? Perhaps AD5942BATZ does not support measuring body impedance(BIA)?

Thread Notes

Parents
  • Hi there, I was wondering if you’ve managed to solve this problem yet, and if so, how? I’m running into almost exactly the same issue as you: I’m using the ADICUP3029 base board with the EVAL-AD5941BATZ daughter board to measure resistance, but I can’t even get a correct reading on a simple through-hole resistor. The values I’m getting are all way too high.

Reply
  • Hi there, I was wondering if you’ve managed to solve this problem yet, and if so, how? I’m running into almost exactly the same issue as you: I’m using the ADICUP3029 base board with the EVAL-AD5941BATZ daughter board to measure resistance, but I can’t even get a correct reading on a simple through-hole resistor. The values I’m getting are all way too high.

Children
No Data