Post Go back to editing

algorithm program code based on MAX30102 for measuring heart rate and blood oxygen?

Category: Software
Product Number: MAX30102

在使用MAX30102时,我发现测量结果总是不准确。我想可能是我的数据处理方法和算法有问题。我想知道,针对MAX30102这款芯片,厂家有对应的软件支持吗?

When using MAX30102, I found that the measurement results are always inaccurate. I think it may be a problem with my data processing methods and algorithms. I would like to know if the manufacturer has corresponding software support for the MAX30102 chip?

Thread Notes

Parents Reply Children
No Data