Post Go back to editing

输入是扫频信号,IF没有输出

Category: Hardware
Product Number: HMC412B
translator
我在使用HMC412时,LO端口和RF端口都输入8-12G的FMCW波,LO端口功率为10dBm,最终IF端口没有输出,请问这个是硬件本身不可以实现此功能还是我的操作有问题?
Double-click
Select to translate

Hi,
I have some questions about the sweep signal IF port output.The input signal is FMCW.The power of the LO port is 10dBm, and the frequency sweep signal of 8-12G is input. The RF port inputs the frequency sweep signal of 8-12G, but the IF port has no output.

How to make the frequency sweep signal output the correct IF signal?

Thanks!

Thread Notes