Post Go back to editing

ADF4372的相位噪声问题

Category: Hardware
Product Number: ADF4372

目前我在使用ADF4372进行设计,频率输出的要求是8GHz-14GHz, 原理图上使用RF16P作为输出管脚,RF16N通过隔直电容接50Ω到地,目前测试频率9.7GHz,环路带宽在200KHz左右,测试结果如下

但是仿真软件的1KHz-100KHz的相位噪声可以达到-100dBc/Hz以下,我的电荷泵电流设置为最大5.6mA,鉴相频率使用30.72MHz,

下图为30.72MHz的相位噪声

请帮忙看下我测试到的9.7GHz的相位噪声结果有问题吗,如果有问题请帮忙分析一下

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.