Post Go back to editing

芯片外壳材料咨询

Category: Datasheet/Specs
Product Number: MAX30101

我们正在基于MAX30101开发一套穿戴式健康监测设备。我们希望用整体包胶工艺做外壳,这需要确定芯片的外壳材料种类,以确定是否与外壳生产工艺兼容。希望能得到关于MAX30101外壳材料种类的回复。

We are developing a wearable health monitoring device based on MAX30101. We hope to use the overall encapsulation process to make the shell, which requires determining the type of shell material of the chip to determine whether it is compatible with the shell production process.Hope to get a reply on the type of housing material of MAX30101.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.