Post Go back to editing

关于AD9122输出波形的问题

Category: Hardware
Product Number: AD9122

问题描述:我们对AD9122配置完成之后,输入data数据(输入数据见图1),用示波器查看后发现没有像预期显示那样显示出来(示波器测量见图2),对程序进行仿真后是正常输出的状态(仿真图见图3)请问我想要正常输出该如何去做

1 输入数据

2 示波器测量图(黄色为变压器前端,蓝色是变压器后端)

3 仿真图(输入为data_p_outdata_n_out

4 9122手册图

Thread Notes

  • 感谢您的提问!获取更多关于该产品的信息,欢迎您联系术支持  · Support Portal (analog.com)

  • Hi  ,

    抱歉,我遗漏了您的查询. 您能否提供包含您输入到 AD9122 的数据的 .txt 文件?它似乎是一种任意波形(而不是正弦波之类的函数)。您很可能发送的是 2 的补码数据,但 AD9122 中的数据格式设置为无符号二进制(反之亦然)。图 69 仅表示 AD9122 的输出是差分的(即 IOUTP/IOUTN 和 QOUTP/QOUTN),并通过在输出端使用差分变压器或平衡器转换为单端(具有相同的峰值电压,但共模误差源减少)。

    Apologies for missing your query. Can you provide the .txt file containing the data you input to AD9122? It seems it's an arbitrary waveform (as opposed to a function like a sinusoid). It's likely that you are sending 2's complement data but the data format in AD9122 is set to unsigned binary (or vice-versa). Figure 69 only says that the output of AD9122 is differential (i.e. IOUTP/IOUTN and QOUTP/QOUTN), and is converted to single-ended (with the same peak voltage but with the common-mode error sources reduced) by using differential transformers or baluns at the output. 

    Best regards,
    Marco

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.