Post Go back to editing

4-20mA输出电路及采样电路

Category: Hardware
Product Number: AD5410

我现在使用的4-20mA输出电路是AD5410单通道输出电路,未加入HART,4-20mA采样电路是AD8420的推荐电路,电路见附件。

我的需求是:

第一:我需要多通道输出的4-20mA输出电路以控制多个线性阀,我在考虑使用多片AD5410组成菊花链或其他形式,或者使用AD5755-1这款四通道输出的芯片搭建电路,这方面请问有好的建议吗?

第二:对于AD8420组成的4-20mA采样电路,此电路是否可以良好使用?对于采样电路的“地”与电路板(电路板采用数字地和模拟地单点连接)的“地”与传感器的“地”的处理,可以给我一些好的建议吗?

第三:我有两路4-20mA采样电路,所以我想使用多通道的ADC以节省空间和资源,请问我的想法是否合理?对于ADC的选型可以给我一些好的建议吗?

Thread Notes