Category: Hardware
Product Number: AD5410
我想使用AD5410输出4-20mA电流,电路图见附件。问题:板子一上电AD5410的FAULT引脚就输出低电平(图中LED灯FLAUT1亮了,而且按下单片机的复位键这个LED灯也不会灭)。我确信写入寄存器的数据正常,回读正常(写入0x3015,读出也是0x3015),读出状态寄存器的数值DB2-DB0是0x100,根据数据手册,这表示Iout引脚上检测到故障,然而我确定我接入了250欧的负载电阻。测量得到R3_SENSE和BOOST引脚上的电压都是24V,DVCC引脚电压4.6V,REFIN和REFOUT电压5V,I_OUT引脚电压0V。
我试过复位、重新下载程序、输出4mA或者20mA,都没有用处。请问有什么好的建议吗。