English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
如何使MAX9275与MAX9288一起工作?
FAQs
讨论
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
5 months ago
FAQs
MAX
MAX9288GGM/VY+_T1: FAQ
如何使MAX9275与MAX9288一起工作?
如果锁定引脚为高电平表示时钟稳定。 检查以下寄存器:
D4位为0x14 is1,DRS为高电平,即低数据速率模式,参见表5,可以发现最大Pclk为36M,所以需要配置,DRA = 0,BW1 = 1;
0x65 D [5:4])默认值为10,只有D0和D1两位输出,如果改为11,则输出配置为4位
HBP和HFP是70像素,参考图17,MAX9288需要200个。
000094102
MAX9288GGM/VY+
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.