Article 当输入电压低于6V时,MAX17504的内部LDO输出不稳定,原因是什么?

正常情况下,即使输入电压低于6V,MAX17504的内部LDO的输出也应该是稳定的电压,只是当输入电压较低时,内部LDO的输出可能会低于5V。例如,当输入为5V时,LDO的输出可能在4.5V左右,但是MAX17504还是可以正常工作的。造成LDO输出不稳定的原因可能是输出电容过大,启动时的浪涌电流造成LDO无法正常工作,针对这个问题,可以增大软启动电容。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.