Article DS1804-100+ 内部的EEPROM写入次数超过限制后该如何操作?是否器件就无法写入了?

DS1840内部的EEPROM写入次数为50000次,当超过次数后,就无法正确保存写入结果。

 

 

 

DS1840内部有EEPROM和控制单元,在正常使用时,可以通过控制单元任意更改抽头的位置,但是不用写EEPROM,也就是说,上电后,可以更改抽头的位置,比如更改了1000次,但是没有写入EEPROM,如果需要调整下次上电后抽头的位置,可以更改EEPROM,否则就可以不用更改EEPROM,这样即使通过控制单元更改了1000次抽头位置,但并不影响EEPROM的写入次数,因为在更改的过程中没有写入EEPROM。

最常见的应用是初始化时写一次EEPROM用于设定上电后抽头的位置,上电后通过控制单元更改抽头位置,这样即使频繁更改抽头位置,对于EEPROM来讲只是写入了一次。所以50000次是足够使用的。

 

 

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.