English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAXREFDES220#: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAXREFDES
MAXREFDES220#: FAQ
MAXREFDES220#: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAXREFDES220使用时必须静止吗?如果一般性运动(如散步、进食等),测量准确度的变化如何?被测对象应保持什么状态?
必须保持静止。锻炼,说话,饮水或饮食等活动可能会对收缩压产生10mmHg至20mmHg的影响。在测量过程中,被测对象应该坐在舒适的椅子上,不要交叉双腿;手臂应放在桌面上,并和心脏相平;背部应靠在椅背上。如果被测对象的背部不靠在椅背上,则舒张压的测量值可能会增加5mmHg至10mmHg。交叉双腿会使收缩压增加2mmHg至8mmHg。将手臂放置在心脏水平面以下会导致较高的收缩压,而将手臂放置在心脏水平面以上则会导致较低的收缩压…
MAXREFDES220可以用于测量血压趋势,测量值和实际值的误差是多少
MAXREFDES220在使用之前需要校准。经过校准的MAXREFDES220提供业内最佳测量精度,符合II类医疗精度标准。例如,在静态测量条件下,MAXREFDES220可实现如下精度等级: 收缩压误差:均值 = 1.7mmHg,标准差 = 7.4mmHg 舒张压误差:均值 = 0.1mmHg,标准差 = 7.6mmHg 注: II类医疗精度标准为均值绝对值 ≤ 5mmHg…
MAXREFDES220多人轮流使用,是否需要切换校准血压?如果需要针对不同用户切换针对该用户的校准值,这样频繁切换是否影响血压测量精度?
MAXREFDES220的软件本身可以选择多个用户,并存储不同用户的校准值,用户的切换并不会对精度产生任何影响。
MAXREFDES220的血压趋势测量功能是只适用于正常血压用户,还是同时适用于高血压患者?当高血压患者吃药血压恢复正常后,测量的血压趋势能否跟随下来并仍保持在II类器械的误差范围内?目前的PWTT血压算法基本都无法做到这一点。
可以同时适用于高血压用户,包括服药的用户。因为MAXREFDES220的算法不是PWTT算法,PWTT算法是不能跟随服药的高血压患者的。我们的算法仅对PPG的形态进行估计从而测量血压趋势。
关于MAXREFDES220的使用,人的血压一天内有变化,校准血压值是输入晨峰期间血压,还是可以输入一天内任何时段的血压值?在极端情况下,不输入校准血压就使用,准确度会有多大误差?
用户在校准前应静止5分钟,并避免在前30分钟内锻炼,饮用酒精、咖啡因或吸食尼古丁产品。由于MAXREFDES220根据PPG信号的形态学变化,测量的是相对的血压趋势,再根据对应的标准血压校准值计算血压趋势的绝对值,因此只要满足校准条件就可以进行校准。不输入校准血压,不能得出正确的血压趋势值。
在运动状态下能否测量血氧?
血氧不可以在运动状态下测量,因为按照国际标准,血氧是在静止状态下测量的氧合血红蛋白与全部可结合血红蛋白之比。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.