MAX96705AGTG/V+: FAQ

MAX96705AGTG/V+: FAQ
  • Created
Was this helpful?
  • MAX96705的I2C地址如何定义?

    MAX96705有两组I2C地址映射寄存器,分为I2C_sourceA,I2C_destA和I2C_sourceB,I2C_destB。每组中,I2C_dest用于存放MAX96705所连接器件的实际I2C地址,I2C_source用于存放用户赋给该器件的地址。这两组寄存器的作用是在有多个I2C器件挂接在同一总线时,避免地址冲突。
  • 在GMSL1设计中,POC滤波电路中的330nH电感很容易烧坏,为什么?

    在GMSL的PoC供电电路中,我们推荐了3电感滤波器。其中电感的额定电流为500mA左右,如果出现电感烧坏现象,请确认电感的额定电流是多大;如果电感具有足够的额定电流,应检查电路中是否存在其他产生较大浪涌电流的隐患。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.