English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX9288GGM/VY+_T1: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX9288GGM/VY+_T1: FAQ
MAX9288GGM/VY+_T1: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAX9271是否能与MAX9288配对使用?
MAX9271可以与MAX9288配对,但是是有条件的,MAX9271和MAX9288只能工作在single mode,不能工作在double mode。这一点与MAX96705不同,原因是MAX96705有crossbar功能,可以在double模式下进行double allignment, 而MAX9271没有crossbar功能。
如何使MAX9275与MAX9288一起工作?
如果锁定引脚为高电平表示时钟稳定。 检查以下寄存器: D4位为0x14 is1,DRS为高电平,即低数据速率模式,参见表5,可以发现最大Pclk为36M,所以需要配置,DRA = 0,BW1 = 1; 0x65 D [5:4])默认值为10,只有D0和D1两位输出,如果改为11,则输出配置为4位 HBP和HFP是70像素,参考图17,MAX9288需要200个。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.