English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX7317: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX7317: FAQ
MAX7317: FAQ
MAX7317
I/O Port Expanders
Created
over 8 years ago
Updated
13 days ago
Was this helpful?
Yes
No
More
Cancel
MAX7317 SPI通信波形正确。但是IO口输出始终为高电平,是什么原因?
首先要确定SPI通信模式,SPI通信有四种模式,分别为时钟极性与时钟相位分别为0,1的情况。MAX7317 极性为0(CLK默认低电平)相位为0(CLK时钟第一个上跳沿读取数据) 如果SPI通信没有问题,而IO状态还是没有改变,那么注意到IO口为开漏极输出,根据其Sink Current=0.5mA,供电电压3.3V计算,上拉电阻应大于6.6K,选用10k上拉电阻即可。过小、过大的上拉电阻不会得合理的IO输出…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.