MAX5974AATE+: FAQ

MAX5974AATE+: FAQ
  • Created
Was this helpful?
  • MAX5969AEVKIT的输出电流如何增加至2A?

    MAX5969AEVKIT的板子上预留了一个封装为SOT23的MOSFET,N3是和输出整流MOSFET N2并联的,根据MAX5969AEVKIT的datasheet,增加这个MOSFET并将工作频率提高至400kHz可以将输出电流由1A增加至2A。需要注意的是,除了增加这个MOSFET,还需要增加这个MOSFET的驱动电阻R56,可以使用10欧姆的电阻。而由于输出功率增加了,前面MAX5969A的分级电阻要由43…
  • MAX5974A close loop gain test

    MAX5974A不能测环路的情况是指MAX5974A电感绕组反馈方案情况,如果MAX5974A用的是光耦反馈还是可以测环路的,和MAX5974D一样方式测。 在用电感反馈时,MAX5974A采用的是采样保持电路进行反馈,简单的讲就是一个周期只采样一个点,把这个点的电压作为反馈信号进行pwm调制,那么当你用bode仪注入信号时,芯片不一定能看到这个扰动,故而无法测试。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.