MAX32664GTGA+: FAQ

MAX32664GTGA+: FAQ
  • Created
Was this helpful?
  • MAX30102、MAX30001等光学传感器或者是生物电势传感器是否自带算法?

    Maxim的大多数传感器都不具备算法功能,但是我们提供算法传感器集中器供客户选用。其中,MAX32664A或MAX32664D搭配指尖式光学传感器模组MAX30101或MAX30102;MAX32664B或MAX32664C搭配腕带式光学传感器MAX86140或MAX86141;MAX32664C还可以搭配入耳式光学传感器模组MAXM86161。MAX32663A可以搭配心电及生物电阻抗传感器MAX30001…
  • MAX32664是否可以外接显示屏

    关于MAX32664,其本身只是个传感器集中器,并不是MCU,还是需要一个主MCU去控制MAX32664的,可以将显示屏、蓝牙等等外设挂在主MCU上。主MCU的型号可自选。
  • MAX32664是否支持除了MAX30101/2、MAX86140/1以外的传感器

    MAX32664有四个版本。MAX32664版本A支持MAX30101、MAX30102,适用于基于手指的可穿戴健康应用,用于监测心率和血氧。 MAX32664版本B支持MAX86140、MAX86141,适用于基于手腕的生命体征监测,用于监测心率。 MAX32664版本C和版本B类似,在版本B具备的心率监测功能上增加了血氧功能。 MAX32664版本D是版本A的加强版,除了心率…
  • MAX32664的四个版本应用场景是什么?

    MAX32664有四个版本。MAX32664版本A支持MAX30101、MAX30102,适合基于手指的可穿戴健康应用,用于监测心率和血氧;MAX32664版本B支持MAX86140、MAX86141,适合基于手腕的生命体征监测,用于监测心率。MAX32664版本C和版本B类似,在版本B具备的心率监测功能上增加了血氧功能。MAX32664版本D是版本A的加强版,除了心率、血氧,还可以用来监测血压。因此…
  • 使用MAX32664后,PPG芯片需要满足什么样的限制?比如是否有固定型号的LED/PD及感测位置?若后端再接一个MCU,软件如何控制?

    MAX32664的版本A和D支持MAX30101、MAX30102,这两个器件是模组,所以LED和PD都封装在芯片里面了。版本B和C支持MAX86140、MAX86141,这两个器件需要自行选用PD和LED,型号可以根据数据手册,选择合适的即可。关于PD和LED的分布位置,及光学设计部分,我们有相关的技术文档提供,具体请联系技术支持。MAX32664是需要作为从机和主机通信的,一般是主机控制MAX32664读取数据…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.