English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX31790ATI+T: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX31790ATI+T: FAQ
MAX31790ATI+T: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX31790 Theta Jc和Theta Ja分别是多少?
Theta Jc= 3C/W Theta Ja=48C/W
MAX31790数据手册V2版在介绍TACH引脚的说明时,提到:For a 2-wire fan, analog input can be used for fan-failure detection,这个怎么理解?
此处的说明是一个错误,首先TACH引脚只能接收逻辑信号(高或者低),无法支持模拟信号,对于2线制风扇,只有电源和地,无法和MAX31790的TACH引脚连接,应该是对3线制或者4线制风扇而言,并非2线制风扇。
MAX31790是否适用30000RPM转速风扇的监控,手册中只提到16000RPM?
MAX31790在计算转速时,最好采用4线制风扇,如果是3线制风扇,要设计为PWM调整电源电压的工作方式(见数据手册Figure9,Figure10). 风扇转速是通过对内部时钟信号进行计数来实现的,计数时间由选择的转速计脉冲个数来确定,也就是说,转速越高,计数时间越短,转速越慢,计数时间就越长。所以在最高速度时,要选择最多的转速计脉冲,但是当风扇速度降低后,计数时间就会bian长,这样就会限制最低的转速…
max31790风扇控制芯片控制3线制风扇,采用PWM控制,风扇地 与GND之间的MOS管通断 来进行风扇调速,因为 mos管不断的开启断开,风扇的地不断的浮空 导致转速信号采集错误。有好的解决办法吗
这个问题对于三线制风扇的确是存在的,对于三线制的风扇,此时不能直接通过MOSFET来控制风扇的转速,如果风扇的最大电流比较小,比如200mA--300mA, 那么可以采用数据手册中图9的电路,将PWM信号转换成直流电压信号控制施加到风扇的电源电压,从而达到调速的目的。如果风扇的电流比较大,则需要采用外部DC-DC电源模块来调节风扇的电源电压以实现调速,数据手册Figure 10 给出了一个利用DC…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.