English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX30205EVKIT#: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX30205EVKIT#: FAQ
MAX30205EVKIT#: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX30205数据手册与MAX30205EVSYS数据手册推荐了不同的采样率,请确认哪一个是正确的?
MAX30205EVSYS数据手册(Rev.0)中给出的“10sps”应改为10s,以消除器件自热引起的测温误差。另外,MAX30205 GUI
MAX30205是接触式测温吗?
max30205是通过和被测部位/环境紧密接触实现测量的,为了保证测量效果,需要将芯片背面的导热体和被测部位紧密接触。
MAX30205测量体温时如何减少环境影响?
MAX30205用于测量体温,为减少环境温度对它的影响,可以用绝缘胶或塑料隔离与周围环境的热传导,只保留测量部位与被测物体/热源的接触。请参考下图安装示意图:
使用数字温度传感器MAX30205,将传感器芯片用导热硅胶固定在铁片上置于恒温箱,恒温箱设定40℃,测试芯片从室温28℃升到39℃需要3分钟,39℃升到39.8℃需要30分钟,最后在39.8℃附件徘徊,请问MAX30205温升速度能否提升,温度比实际温度低是否可以解决?
普通导热硅胶的热导率太低,通常我们推荐用热导率高的物质将器件下方的裸焊盘和测温点接触,如果用PCB板焊接MAX30205,可以在MAX30205下方打一个过孔,在过孔中添焊锡,也可以用导热率高的胶进行连接,我们推荐的产品有如下几种: https://www.appli-tec.com/ https://www.masterbond.com/ https://www.3m.com…
手册中给出的MAX30205 Iq指标为600uA时,AFE是什么状态?
手册中的IQ是600uA时,I2C接口待机,而AFE是工作状态;1.65uA静态电流则指关断模式下的电流,AFE不工作。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.