English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX30102EFD+T: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX30102EFD+T: FAQ
MAX30102EFD+T: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAX30102 I2C电平与IC供电可以不同吗
I2C接口的SCLK和SDA均为漏极开路,需要外部上拉电阻器将总线电压上拉至所需的电压水平。I2C电平则与其相应引脚电压耐受有关,MAX30102的I2C引脚最大可承受6V电压。
MAX30102 SHDN功能怎么用?
只需配置Mode Configuration (0x09)的最高位即可,1为关断模式,0为使能。进入关断模式后,所有寄存器的值都维持原数据。重新使能之后可以继续使用。
MAX30102可以在远距离实现血氧饱和度的测量吗?
问题: MAX30102能不能在远距离,如5cm,实现对血氧饱和度的测量?或者有没有其他类似的产品可以满足这种需求(在2-5cm距离处测量血氧),偏差大至±2%可以接收? 回答: 按照国际标准,血氧测量需要将组织和芯片紧密接触,2-5cm的距离难以获得血氧值。
MAX30102的I2C接口需要上拉到几伏?
I2C接口需要上拉为和Host MCU相同的接口电平。 这里MAX30102的I2C接口是可以上拉到5V的。
MAX30102的Multi-LED mode 有什么作用?
从数据手册Page15可以看出每一个采样样本包含两个部分,红光和红外,采样结果各3个字节。 选用Multi-LED 模式的情况下每个样本划分成4个部分,每部分3个字节。 4 个部分的构成可以自定义。例如定义为3个来自红光的结果,一个来自IR的结果等等。 可以更加灵活的配置采样,调整测量结果。
MAX30102的R_DRV和 IR_DRV的作用是什么?如何连接?
它们是IR和RED的驱动,不需要外部连接,内部已经连接好了。
MAX30102血氧芯片在使用中是否需要另外加玻璃外罩,如果加玻璃外罩有什么要求
如果加玻璃外罩是没有问题的。但是需要注意的是所加玻璃外罩必须保证对红光红外的透光率大于90%,否则会使采集到的信号不准确。
MAX30102采样率是否可以任意设置?
采样率可以设置成数据手册中列出的8个固定采样率,不能任意设置其它的值,不能自定义采样率。
MAX86160能否测试SpO2?
MAX86160集成了IR和Green LED, 可以测量HR,不能测量SpO2, 重点是可以用于耳朵处测量。
MAXREFDES117#对供电电源的要求是什么?
MAXREFDES117#的输入电压可在2V至5.5V范围内变化,但输入电流必须是1.5mA。1.5mA供电电流一般可由3.3V输入电压产生,取决于连接到Vin引脚的微控制器。
>
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.