English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX30001EVSYS#: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX30001EVSYS#: FAQ
MAX30001EVSYS#: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
使用MAX30001EVSYS测量时,为什么会在一个起搏信号下面标示出两个上升沿和下降沿?
为了获得准确的起搏信号检测,需要正确设置寄存器PACE_DACP和PACE_DACN的值,PACE_DACP和PACE_DACN设置了上升和下降边缘的阈值。阈值太小会导致识别出多余的起搏信号。
使用MAX30001EVSYS测量的时候,输出信号的幅度为什么小于输入心电信号的幅度(假设输入信号为1mV,则输出信号只有大约0.85mV)?
心电信号是微弱信号,因此在从体表经过电极、导联线等传导路径到传感器,会发生一定衰减,这是正常现象。如果使用内部校准(internal calibration)功能生成一个1mV的心电信号直接内部进行转换,可以发现输出信号的幅度就是1mV,这说明MAX30001本身不会对信号造成较大衰减,而是传导路径对信号造成了一定衰减。
在MAX30001EVSYS的GUI软件里面调整PGA的通道增益,为什么在GUI端输出的心电波形的幅度不变?
GUI输出波形的幅度和实际输入波形的幅度是要保持一致的,不受PGA增益设置的影响。 MAX30001的PGA的增益是用于内部放大的,以便适应ADC的输入电压范围。GUI内部的算法会把PGA增益变化的影响给消除掉,从而使得GUI输出波形的幅度和实际输入波形的幅度是要保持一致的。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.