MAX2870ETJ+: FAQ

MAX2870ETJ+: FAQ
  • Created
Was this helpful?
  • MAX2870小数模式下杂散远远大于整数模式下的杂散,为什么?

    关于MAX2870,分数模式下,将CPL = 1 有助于降低杂散,请确认以下寄存器配置: Register 1, CPL[1:0]: 01 = Enables the CP linearity mode (frac-N mode)
  • MAX2870的数字输入逻辑电平范围是多少?

    MAX2870数字逻辑电路由VCC_DIG引脚供电,该电源的有效输入电压范围为+3.0V至+3.6V,容限为+/-10%的+3.3V输入电源。所有引脚的绝对最大电压为VCC_ + 0.3V。评估板原理图在微控制器与MAX2870之间有电平转换器,因为微控制器直接由+5V USB输入供电,MAX2870由用户提供的+3.3V电源供电。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.