English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX2829ETN+: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX2829ETN+: FAQ
MAX2829ETN+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX2829如何通过SPI修改接收工作频点(5G频段)?
5GHz模式下,由于较宽的调谐范围,MAX2829需要启动内部的FSM(有限状态机)选择子频段;当然,也可以通过SPI写入子频段。如果使用FSM选择,则需操作以下步骤: 1) 设置D8 = 0 (A3:A0 = 0101)使能FSM自动选择VCO子波段; 2) 需要的话,使能PLL和VCO,编程分频比; 3) 设置D7 = 1 (A3:A0 = 0101)启动FSM。FSM应在PLL和VCO使能后…
使用SPI接口控制RX/TX增益时,如何处理MAX2829的B1-B7输入?
使用SPI接口设置RX/TX增益控制时,使输入B1-B7保持浮空。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.