English
EngineerZone
Other Products (CN)
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
Other Products (CN)
FAQs
MAX2771ETI+: FAQ
FAQs
讨论
Tags
Cancel
FAQs
MAX
MAX2771ETI+: FAQ
MAX2771ETI+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX2769内部集成了2个低噪放,可以连接有源或无源天线,MAX2771只有一个低噪放,是否可以连接无源天线?
MAX2771内部两个低噪放分别用于L1波段和L2/L5波段信号放大,可以连接无源天线。 MX2769内部的LNA1提供更高增益,优化与无源天线连接;LNA2增益略低,具有更低的噪声系数并且内置50欧姆匹配。MAX2771内部L1波段低噪放特性与MAX2769的LNA1近似,适用于无源天线连接,不需要额外增加低噪放。
MAX2771 ADC的最高采样速率是多少?
MAX2771 ADC的最高采样速率是50MHz,但工作在此采样率时,需要提供外部采样时钟。
MAX2771 PLL的锁相时间是多少?
MAX2771数据手册没有提供PLL的锁相时间,因为该时间与参考时钟启动时间、PLL整数/分数分频比设置、外部环路滤波等因素有关。客户完整设计后,可以通过LD引脚测量锁相时间。
MAX2771在shutdown模式下,是否可以配置寄存器?
MAX2771可以通过0x00寄存器的CHIPEN位,或者把SHDN引脚拉低进入shutdown模式。无论yi哪种方式进入shutdown模式下,SPI接口功能依然保持,可以配置寄存器。
MAX2771是否可以同时接收L1、L2波段信号?
MAX2771支持多波段卫星信号接收,但不能同时支持多个波段(比如:L1、l2)卫星信号的接收,其内部虽然提供独立的L1和L2/L5 RF模拟前端,但基带部分是共用的。
MAX2771是否支持M码?
MAX2771配合适当的基带处理器,对收到的GPS信号进行解调,可以支持M码。但其上一代GPS接收器MAX2769C则不支持。
MAX2771环路滤波器电路
MAX2771环路滤波器采用3阶低通滤波,电路如下: R3、C3集成在MAX2771内部,产生第3个极点。低通滤波器带宽通常为几十kHz,频带越宽,锁相时间越短,但杂散信号越大。
max2771的内部ADC时钟和CLK_OUT有相位差吗
CLK_OUT和CLK_ADC之间有相位差。
MAX2771评估板测试中,一旦采用小数分频,则在输出杂散明显增大,原因是什么?
锁相环的相位噪声与分频比相关,使用整数分频时,相位噪声与整数分频比N成正比:20 x log (N)。N越大(PFD频率越低)相位噪声越大。 到分频比为小数时,分频反馈环路的∑-∆调制器使能,将引入额外的相位噪声(抖动),在输出端产生的杂散信号也越大。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.