Is there a driver for the AD7768 for the Zephyr system? Or is there a plan to develop a driver for the AD7768 on the Zephyr platform?
Zephyr is a relatively new operating system for embedded systems, somewhat similar to Linux. Currently, the AD7768 project is used in two products: one is on the single-chip microcontroller STM32H753, which is a Zephyr system; the other product is on the RK3588, where the AD7768 is connected through an FPGA.