Post Go back to editing

adxl1002 输出波动问题

ADXL1002 设计图:

使用示波器测量  R2 电阻输出端的模拟信号,在静止不动的状态下,输出的波动超过了25mv(1g),峰峰值有80mv,这可能是什么原因造成的?

  • 从输出波形来看,出现了很大的约0.5us(200MHz)的高频振荡波形,

    1、首先请您用手拨一拨示波器探头,这个波形是否会发生变化?如果变化有可能是示波器探头自身引入?

    2、是所有产品都出现这个问题,还是只是这一块板子出现了这个问题?

    3、这个板子上面的GND是否和其他数字GND公用了?特别是MCU的I2C/SPI等的数字地,因为IC本身是输出模拟信号,所以请将两个地分开

    4、请对IC施加自检(self-test),看看输出是否相应地电压?若可以输出电压,说明此振荡是外部引入的。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.