Post Go back to editing

ADXL367设置FIFO采样长度后,使用轮询方式1s读取一次(非中断),但和预期的不一致

Thread Summary

The user is experiencing an issue with the ADXL367 FIFO in stream mode, where 513 data entries are read instead of the expected 64. The final answer clarifies that FIFO_SAMPLES does not control the FIFO depth but only the watermark interrupt threshold. To achieve the desired functionality, the user should read only the first 64 data entries from the FIFO, ignoring older data.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADXL367

I use the FIFO of ADXL367 and set it to stream mode, hoping to save 64 sets of X, Y, and Z-axis data with a sampling frequency of 400Hz. I poll the FIFO data every 1 second (without using interrupts), but I always find 513 data entries when reading the FIFO, which is inconsistent with the manual description. How should I configure it to achieve my desired functionality?

我使用ADXL367的FIFO,并设置为流模式;采样频率为400Hz,FIFO长度设置为64;我每隔1s轮询读取FIFO中的数据(不使用中断) ,但是我发现FIFO中总是513、512条数据,不是我预期的64个数据;有什么方式可以实现我的功能吗?

this is my code 

uint16_t adx1367_get_fifo_xyz(uint16_t *buff)
{
uint8_t data_buff[512 * 2] = {0};
uint16_t fifo_entries = 0;
uint8_t reg_val[2] = {0};

adxl367_get_register_value(&reg_val[0], ADXL367_REG_STATUS, 1);
if(reg_val[0] & 1 << 2){
adxl367_get_register_value(reg_val, ADXL367_REG_FIFO_ENTRIES_L, 2);
fifo_entries = ((reg_val[1] & 0x03) << 8) | reg_val[0];
if((0 == fifo_entries)){
return 0;
}

adxl367_get_register_value(data_buff, ADXL367_REG_I2C_FIFO_DATA, fifo_entries);
fifo_entries = (fifo_entries > SAMPLE_DEFAULT_AXI_HZ*6 ? SAMPLE_DEFAULT_AXI_HZ*6:fifo_entries);
for(int index = 0; index < fifo_entries; index++){
buff[index] = (data_buff[index * 2] << 6) + (data_buff[index*2 + 1] >> 2);
}
return fifo_entries;
}

return 0;
}

void adxl367_fifo_setup(void)
{
sample_mode_info_t *p_sample = NULL;
uint8_t reg_value = 0;

p_sample = sample_config_get();

// Set fifo stream mode
adxl367_get_register_value(&reg_value, ADXL367_REG_FIFO_CONTROL, 1);
reg_value &= ~(3);
reg_value |= ADXL367_STREAM_MODE;

// Set fifo sample x,y,z
reg_value &= ~(0x0F << 3);

// set fifo sample 64/1
reg_value &= ~(1 << 2);
adxl367_set_register_value(reg_value, ADXL367_REG_FIFO_CONTROL);


// set fifo sample 64/1
reg_value = 0;
adxl367_get_register_value(&reg_value, ADXL367_REG_FIFO_SAMPLES, 1);
reg_value = p_sample->sample_axi_hz;
adxl367_set_register_value(reg_value, ADXL367_REG_FIFO_SAMPLES);
}

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.