Post Go back to editing

adxl355读数异常,三轴中某一轴数据始终为0

Contains AI Generated Content

Thread Summary

The user encountered an issue with ADXL355 devices where one axis reads 0 after disassembly and reassembly, while the other two axes function normally. The final answer suggests performing a power-on self-test to check if the devices are still functional. If the self-test fails, the devices may be damaged.
AI Generated Content
Category: Hardware
Product Number: ADXL355

adxl355芯片,我这边做了一批设备,一开始全部工作正常,后续有一次经拆装后,个别出现了三轴中某一轴读数全为0的情况,其余两轴读数正常(还有一个是xz轴异常,y轴正常,其余的为X轴异常,yz正常或z轴异常,xy正常),请问出现这种现象可能的原因是什么?拆装过程中过大的外部激励是否会导致这种现象,以及有什么解决方法?