Post Go back to editing

ADXL355 各轴正反向输出不一致

Thread Summary

The user observed inconsistent absolute values in the output of a 3-axis accelerometer when the chip was placed in different orientations. The final answer indicates this is due to offset, a fixed deviation in the sensor readings, which can be corrected through calibration. The ADXL accelerometer series is referenced for best engineering practices in calibration and usage.
AI Generated Content

供电传感器整体由3V3供电,以SPI通信,量程正负2g,测量时静止放置。

目标:①查明出现芯片按照各轴朝向正反放置时,输出结果绝对值不一致;②解决前述问题;

测量Z轴: 

芯片朝上放置

X= 0.01281208m/s^2, Y= -0.08436847m/s^2, Z= 9.89176369m/s^2, T= 31187.84570312mC
X= 0.00979072m/s^2, Y= -0.07564861m/s^2, Z= 9.87960148m/s^2, T= 31408.83984375mC
X= 0.01147350m/s^2, Y= -0.08368006m/s^2, Z= 9.88954544m/s^2, T= 31298.34179688mC
X= 0.01112930m/s^2, Y= -0.08945505m/s^2, Z= 9.88633251m/s^2, T= 31519.33789062mC

芯片朝下放置

X= 0.50640208m/s^2, Y= -0.06210988m/s^2, Z= -10.28599262m/s^2, T= 32292.81835938mC
X= 0.49576992m/s^2, Y= -0.07859347m/s^2, Z= -10.31054592m/s^2, T= 32403.31445312mC
X= 0.49856183m/s^2, Y= -0.07974082m/s^2, Z= -10.32301426m/s^2, T= 32292.81835938mC
X= 0.50299823m/s^2, Y= -0.07576334m/s^2, Z= -10.30610943m/s^2, T= 32292.81835938mC
X= 0.49821761m/s^2, Y= -0.08234148m/s^2, Z= -10.29976082m/s^2, T= 32292.81835938mC

测量Y轴: 

芯片侧放

X= -0.04428771m/s^2, Y= -10.10444355m/s^2, Z= 0.06126849m/s^2, T= 31961.32617188mC
X= -0.03086372m/s^2, Y= -10.10318184m/s^2, Z= 0.06073306m/s^2, T= 31850.82812500mC
X= -0.02952514m/s^2, Y= -10.10677624m/s^2, Z= 0.05461386m/s^2, T= 31961.32617188mC
X= -0.03920113m/s^2, Y= -10.10765648m/s^2, Z= 0.07293322m/s^2, T= 31961.32617188mC

芯片侧放

X= 0.06834382m/s^2, Y= 9.90725231m/s^2, Z= -0.65899962m/s^2, T= 32071.82421875mC
X= 0.06784663m/s^2, Y= 9.91298962m/s^2, Z= -0.66236520m/s^2, T= 32071.82421875mC
X= 0.06337196m/s^2, Y= 9.92465401m/s^2, Z= -0.68393534m/s^2, T= 32182.32031250mC
X= 0.07400407m/s^2, Y= 9.91620159m/s^2, Z= -0.67594212m/s^2, T= 32182.32031250mC

测量X轴: 

芯片侧放

X= 9.87218189m/s^2, Y= -0.46559462m/s^2, Z= 0.12934460m/s^2, T= 34723.75781250mC
X= 9.86927509m/s^2, Y= -0.46242028m/s^2, Z= 0.10437061m/s^2, T= 34723.75781250mC
X= 9.89141941m/s^2, Y= -0.45385340m/s^2, Z= 0.09783071m/s^2, T= 34723.75781250mC
X= 9.88878059m/s^2, Y= -0.44203570m/s^2, Z= 0.09400621m/s^2, T= 34723.75781250mC

芯片侧放

X= -9.88097858m/s^2, Y= 0.00921705m/s^2, Z= -0.50521642m/s^2, T= 33176.79687500mC
X= -9.87757397m/s^2, Y= 0.01028791m/s^2, Z= -0.51435697m/s^2, T= 33287.29296875mC
X= -9.87309933m/s^2, Y= 0.01629237m/s^2, Z= -0.50873500m/s^2, T= 33287.29296875mC
X= -9.87646484m/s^2, Y= 0.02076704m/s^2, Z= -0.51083845m/s^2, T= 33287.29296875mC

通过观察上述测量结果:

①反向放置和正向放置时Z轴的输出绝对值不一致且相差较大 -10.32301426, 9.89176369。

②侧放时Y轴的输出绝对值不一致且相差较大 -10.10765648,9.92465401。

③侧放时X轴的输出绝对值基本一致9.88097858,9.87218189(符合当地的重力加速度)。

④X,Y,Z轴各自的的输出绝对值不一致

为什么回出现如上的现象呢,如何解决呢

Parents Reply Children
No Data