Post Go back to editing

ADXL超过量程时读数小的问题

Thread Summary

用户在使用ADXL362进行400Hz方波振动测试时,发现当加速度超过±8g量程时,读数异常减小,甚至低于5g。最终确认这是ADXL362的正常现象,旧版规格书提到超量程会裁剪为满量程值0x0FFF。建议考虑使用量程更大的ADXL375,以避免此问题。
AI Generated Content

我们用搭载ADXL362的样机去进行方波振动测试,设置的400Hz,量程±8g,在|7g|以内的测试结果都比较正常(还未精确校准所以会有点误差但能接受),但在|8g|和大于|8g|(只测到-9g)的测试时发现读数没有固定在|8g|,反而随着振动加速度的增大,读数变小了,甚至会小于5g。我们需要将大于6g的值作为一个危险信号,如果在高g时读到的值小于5g,那对我们的产品来说是完全不可接受的。请问这是mems加速度传感器的特性还是会有其他因素导致这个问题?

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.