Category: Hardware
Product Number: AD8495
您好,我在使用AD8495芯片+K型热电偶搭建温度采样电路时遇到一些问题,希望能得到您的帮助,问题如下:
我们制作的温度采样电路的原理图如下所示:前端采用建议的滤波电路,在AD8495输出端连接二阶低通滤波电路以及放大电路以放大其输出电压,降低ADC采样精度低干扰。
问题1:在所制作的PCB板中,有一些通道输出电压为震荡信号,但有一些信号输出较为正常。上图仅展示了ADIN3通道的原理图,所制样板中共有4路,电路结构相同。其中测试时AD8495芯片输出正常,但运放输出电压为震荡的信号,将运放反馈回路中0.1uf电容去除后其输出电压较为正常,想问下您这里震荡的原因是什么,以及如何可以避免,谢谢。下图为将AD8495输入引脚采用细铜条短接即输出芯片温度对应电压时的运放电路输出电压波形。
问题2:同样在将AD8495输入引脚短接后,AD8495的输出电压并非稳定的直流信号,而是有一定的扰动,其输出波形如下所示。这里已断开AD8495后级的滤波与放大电路,AD8495输入端滤波电路的电阻已测试100和7.5k,但其输出波形并无明显改善,扰动周期约为2us。想咨询一下这里的扰动产生原因为什么以及如何能将其去除得到较为稳定的直流信号,谢谢。