Post Go back to editing

EVAL-CN0539-E1BZ

Hello, I see from the circuit notes ( from CN0359 site ) that:

if the two-electrode measurement scheme is adopted, the conductivity cell constant is generally 0.1/cm~1/cm.

If the four-electrode measurement scheme is used, the conductivity cell constant is generally 1/cm~10/cm.

However, one of the four electrodes I am currently using is LFS1710 of IST Company. The conductivity cell constant given in its datasheet is 0.44/cm.

During the actual measurement, the development board of CN0359 also gave an alarm sound, resulting in an error in measurement.

I would like to ask if there is any way ( from software or hardware ) to adapt my current electrode. thank you very much.

Parents Reply Children