Post Go back to editing

ADXRS645,想了解如下问题: Vratio引脚电压(F2引脚),不是供电电压,手册中没有规定,看起来只是一个输出参考电压。 Vratio引脚在数据手册中推荐采用的是+5V电压,我能够用+2.5V的电压吗?

Thread Summary

用户询问ADXRS645的Vratio引脚是否可以使用+2.5V电压。最终答案是可以在环境温度下使用+2.5V,但在低温环境下可能存在问题,因为设备阈值电压会增加。如果应用涉及宽温度范围,建议使用V_ratio = 5V。
AI Generated Content

ADXRS645,想了解如下问题: Vratio引脚电压(F2引脚),不是供电电压,手册中没有规定,看起来只是一个输出参考电压。 Vratio引脚在数据手册中推荐采用的是+5V电压,我能够用+2.5V的电压吗?

  • 请参考产线详细的建议和回复:

    “As far as the minimum V_Ratio level, the issue is at cold where device threshold voltages increase.  At 2.5V Vratio, you’ll be just ok at ambient.  Going cold, a stage that feeds the aforementioned Multiplier may drop out.  The XRS645 was intended for downhole applications where high temperature is the norm.  If this is the case, you’ll avoid going cold.  But it all depends on the application. “

     

    So it the customer is planning to use the part in a wide temp range I would stick with V_ratio = 5V.

    请问您是否是有用量信息的企业用户,如果是的话请发邮件到cic.china@analog.com,我们会为您安排线下支持。