Post Go back to editing

ADXL345加速度传感器低温下数据有误

Thread Summary

The user reported that ADXL345 accelerometers on different PCBs exhibit incorrect x,y-axis data at low temperatures (below 0°C), while data is normal at room temperature. Swapping the ADXL345 chips between the PCBs confirmed the issue is with the chips themselves. The final answer suggests closing the problem without providing a specific solution.
AI Generated Content

有个别芯片,在平放状态下,常温时x,y,z轴的加速度数据都是正常。但是当温度较低时,例如低于0度时,x,y,轴的数据开始跳变成一个很大的值(此时依旧是平放),当把温度升高,又恢复正常了,经过多次循环高低温测试,常温下都是正常的,一到低温数据就是错的。为了验证是芯片而不是PCB的问题,我们拿了一个低温下加速度数据正常的PCB和不正常的PCB上的ADXL345加速度计互换位置,此时两个板子的结果也互换了。说明是芯片本身的问题。想知道这种情况是否有解决方案?