Post Go back to editing

How ADXL354 Calculates Bandwidth and Sample Rate Correctly to Obtain Low Noise

Thread Summary

The user is experiencing higher noise levels than expected when using the EVAL-ADXL354 with the ADS1256 ADC. The final answer suggests using the AD7682 with V1P8ANA for voltage reference to reduce noise, and notes that the ADXL354 has an internal low-pass filter of 1500Hz. The user should also consider averaging ADC samples to lower noise, and recognize that the ADC sampling rate forms a low-pass filter at ODR/2. For 20Hz seismic measurements, a 24-bit ADC may not be necessary, and the user is advised to contact Analog Devices support for further assistance.
AI Generated Content

I have an EVAL-ADXL354 and am using the ADS1256 for signal sampling.
Figure (1).

I don't understand how the so called noise density is calculated.

I found this formula " Noise = Noise Density * sqrt(C * 1.6)"

What I want to ask is, does the BW in the formula refer to the frequency width between DCHz and (Low Pass) Hz? Or does it depend on the Sample Rate of the ADC?

If it refers to frequency width between DCHz and (Low Pass) Hz, then EVAL-ADXL354 itself has a 32K internal resistance and an external 0.1uf capacitor, so the bandwidth (BW) is DCHz-49.8Hz.So "Noise = 20ug * sqrt(49.8Hz * 1.6)" = 178.5ug=0.000178g= 1.75×10^-3 m/s²=0.175cm/s2

So why does the noise floor of the data I observe fall about 0.6cm/s2s(ADS125 Sample Rate 100) 0.9 cm/s2s (ADS125  Sample Rate 500)

What am I thinking wrong? Or do you think the reference voltage is unstable or the ADC itself has too much noise?

sorry i really don't understand~

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.