Post Go back to editing

关于ADXL345采集频率不准问题咨询

社区专家好,我在使用345采集振动信号的开发过程中发现,采集标准振动台数据时,采集得到的信号经过FFT分析,信号频率与振动台频率有偏差。 ±16g量程、13位全分辨率、3200/1600ODR,得到的波形为正弦波没有问题,幅值精度也能再1%以内,但是160Hz正弦波实际采集出来的频率为155.5Hz左右(频谱分析),采集100Hz正弦波实际采集出来的频率为96.88Hz左右,用示波器观察345的中断频率也存在误差,不是准确的3200或者1600,误差在+3%左右。

以上现象想确认下是否在345内部时钟允许的误差范围内,如果是那我们要调整这块的应用方案。

谢谢!