Post Go back to editing

关于AD22293Z经过ADXL203推荐电路后的比例因子

我使用AD22293Z,也就是ADXL203的5g版本,按照ADXL203参考设计(CN-0189)文档中的图1搭建了一个试验用电路,用5V供电传感器。按照ADXL203的DataSheet的表1所说,AD22293Z的灵敏度是312mV/g,我在参考电路的左端,也就是传感器端用万用表测量,比例因子的确在312mV/g左右。但在参考电路的右端,也就是AD7887的输入端测量,发现传感器在0g时,电压的确是1.7V左右;但传感器在1g是,电压并不是1.7+3.3/5.0×0.312=1.90592V。不知是为何?特请教,谢谢!

Parents
  • FormerMember
    0 FormerMember
on Jul 21, 2015 6:32 AM

对于AD22293来说,在5V供电时,灵敏度是312 mV/g,0g时的输出应该是2.5V。你可以在AD22293的输出端直接测量看0g时输出是否为2.5V, 1g 或 -1g时是否为 2.5V +/- 312mV。而后再看信号调理后的输出,这样可以确定问题是在哪发生的。

Reply
  • FormerMember
    0 FormerMember
on Jul 21, 2015 6:32 AM

对于AD22293来说,在5V供电时,灵敏度是312 mV/g,0g时的输出应该是2.5V。你可以在AD22293的输出端直接测量看0g时输出是否为2.5V, 1g 或 -1g时是否为 2.5V +/- 312mV。而后再看信号调理后的输出,这样可以确定问题是在哪发生的。

Children
No Data