问题一:我用ADP7102ACPZ-5.0-R7给VDD和AVCC供电5V,用AD586给VRATIO单独供电5V,但是ADXRS620的数据手册中说VRATIO绝对不能高于AVCC,这样就让我很头疼,因为ADP7102ACPZ-5.0-R7生成的5V跟AD586生成的5V都是有误差的,这样就不能100%保证VRATIO不高于AVCC;请问VRATIO是绝对不能高于AVCC还是能稍微高于AVCC?
问题二:为了绝对保证VRATIO<=AVCC,我考虑用AD586给VRATIO和AVCC供电,但是我的系统里有3个ADXRS620,AD586最大输出10mA电流,不知道能否驱的动,另外AD586还要给AD采样芯片的VREF供电,请问ADXRS620的AVCC的最大需求电流是多少?(手册中只说明了VDD\AVCC\VRATIO的总最大电流是4.5mA)。
总上两个问题,我到底应该在ADP7102ACPZ-5.0-R7和AD586的基础上怎样给ADXRS620供电才能保证精度最高?谢谢!