采用ADXL355的芯片来做倾角检测,有个问题请教下:在恒温环境下(直接使用ADXL255内部的温度传感器侦测温度值),上电后校准为X轴和Y轴为0°,然后一直保持供电状态,每10秒输出倾角数据,发现10天后倾角数据会有0.02°左右的漂移,一般是在Y轴,请问零度漂移有这么大吗?如果排除温度的影响,还有哪些可能会导致,谢谢!
采用ADXL355的芯片来做倾角检测,有个问题请教下:在恒温环境下(直接使用ADXL255内部的温度传感器侦测温度值),上电后校准为X轴和Y轴为0°,然后一直保持供电状态,每10秒输出倾角数据,发现10天后倾角数据会有0.02°左右的漂移,一般是在Y轴,请问零度漂移有这么大吗?如果排除温度的影响,还有哪些可能会导致,谢谢!
修改下:在恒温环境下(直接使用ADXL355内部的温度传感器侦测温度值)
请提供一下10天的原始数据信息,发到yiming.zhao@analog.com
请问,你做倾角是使用的那个轴?如何把温度控制到恒定的?精度是多少?传感器在温箱中是如何固定的?发给我数据时,请把环境温度和ADXL355回读的温度一并发回。谢谢。
我们使用ADXL355做的双轴倾角应用,重新架设环境再测试一下,等数据收集好了我发下邮箱给你,到时请帮忙分析下,谢谢!