Dear All:
我想知道如何設置ADcmXL3021 MTC模式嗎? 有任何文件或流程設置規則可以參考嗎? 我需要ADcmXL3021 MTC模式初始SW代碼(initial SW Code),希望為我提供加速的產品開發
Best
Jack
Dear All:
我想知道如何設置ADcmXL3021 MTC模式嗎? 有任何文件或流程設置規則可以參考嗎? 我需要ADcmXL3021 MTC模式初始SW代碼(initial SW Code),希望為我提供加速的產品開發
Best
Jack
The MTC configuration can be found in the DS. We have an evaluation setup that you can test these features with. Here is a link to the wikipage. Here are some examples that can help.
https://github.com/juchong/iSensor-FX3-Firmware
Dear Sir:
This S/W Code only focus Cypress FX3 ,ADI provide open source S/W code to support any one system?? (ex:STM32F xxx ,arduino ,Raspberry Pi)?? thanks
Best
Jack
# adcmxl3021 Driver in Python # SPI Master is using Raspberry Pi # spidev is the Raspberry Pi spi communication library # Date: 2019.7.11 import sys import spidev import time SPI_MAX_SPEED =1953125 class adcmxl3021(): #Configuration Constant based on ADcmXL3021 datasheet PAGE_ID =0x00 TEMP_OUT =0x02 SUPPLY_OUT =0x04 FFT_AVG1 =0x06 FFT_AVG2 =0x08 BUF_PNTR =0x0A REC_PNTR =0x0C X_BUF =0x0E Y_BUF =0x10 Z_BUF =0x12 X_ANULL =0x14 Y_ANULL =0x16 Z_ANULL =0x18 REC_CTRL =0x1A REC_PRD =0x1E ALM_F_LOW =0x20 ALM_F_HIGH =0x22 ALM_X_MAG1 =0x24 ALM_Y_MAG1 =0x26 ALM_Z_MAG1 =0x28 ALM_X_MAG2 =0x2A ALM_Y_MAG2 =0x2C ALM_Z_MAG2 =0x2E ALM_PNTR =0x30 ALM_S_MAG =0x32 ALM_CTRL =0x34 DIO_CTRL =0x36 FILT_CTRL =0x38 AVG_CNT =0x3A DIAG_STAT =0x3C GLOB_CMD =0x3E ALM_X_STAT =0x40 ALM_Y_STAT =0x42 ALM_Z_STAT =0x44 ALM_X_PEAK =0x46 ALM_Y_PEAK =0x48 ALM_Z_PEAK =0x4A TIME_STAMP_L =0x4C TIME_STAMP_H =0x4E REV_DAY =0x52 YEAR_MON =0x54 PROD_ID =0x56 SERIAL_NUM =0x58 USER_SCRATCH =0x5A REC_FLASH_CNT =0x5C MISC_CTRL =0x64 REC_INFO1 =0x66 REC_INFO2 =0x68 REC_PNTR =0x6A ALM_X_FREQ =0x6C ALM_Y_FREQ =0x6E ALM_Z_FREQ =0x70 STAT_PNTR =0x72 X_STASTIC =0x74 Y_STASTIC =0x76 Z_STASTIC =0x78 FUND_FREQ =0x7A FLASH_CNT_L =0x7C FLASH_CNT_H =0x7E PAGE_ID =0x00 def __init__(self, device=0, ce_pin=0): """ device: the SPI device (often 0) ce_pin: pass 0 for CE0, 1 for CE1, etc. device and ce_pin map to device file /dev/spidev{device}.{ce_pin} """ self.spi_init(device, ce_pin) def spi_init(self,device,ce_pin): """ Using "pinout" command to check the raspberry spi definition. device: SPI0 (0), SPI1 (1) ce_pin: CE0 (0), CE1 (1) SPI0 definition CE0 : GPIO8 (0) PIN24 CE1 : GPIO7 (1) PIN26 MOSI: GPIO10 PIN19 MISO: GPIO9 PIN21 SCLK: GPIO11 PIN23 SPI1 definition CE0 : GPIO18 (0) PIN12 CE1 : GPIO17 (1) PIN11PAGE_ID CE2 : GPIO16 (2) PIN36 MOSI: GPIO20 PIN38 MISO: GPIO19 PIN35 SCLK: GPIO21 PIN40 """ # init spi for communication self.spi = spidev.SpiDev() self.spi.open(device, ce_pin) # (x,0) == CE0, (x,1) == CE1 # Set 4-line spi mode self.spi.threewire =False # Set spi msb first self.spi.lsbfirst =False # Set clock phase and polarity to default # SPI_CPOL=0, SPI_CPHA=0 self.spi.mode =3 # Set SPI CS Active Low self.spi.cshigh =False # Set SPI clock rate: 7.8125MHz, cdiv=32, fsclk=250MHz/cdiv, cdiv = [2,4,8,16,32,...32768] self.spi.max_speed_hz=SPI_MAX_SPEED self.spi.bits_per_word =8 def spi_write(self, address, value): # Write value (1 byte) to address # Send instruction (command bit7=1 for write), address[6:0], and value address=address+0x80 self.spi.xfer([address, value]) def spi_write_word(self,address,value_16b): value_l=value_16b & 0xFF value_h=value_16b>>8 self.spi_write(address,value_l) self.spi_write(address+1,value_h) def spi_read_bytes(self, address): # Read # Send instruction (command bit7=0 for read), address bit6:0 rb=self.spi.xfer([address,0],SPI_MAX_SPEED,16,8) return rb def spi_read(self, address): # Read # Send instruction (command bit7=0 for read), address bit6:0 rb=self.spi.xfer([address,0],SPI_MAX_SPEED,16,8) rbc= rb[0]*256 + rb[1] return rbc def spi_read2s(self, address): # Read # Send instruction (command bit7=0 for read), address bit6:0 rb=self.spi.xfer([address,0],SPI_MAX_SPEED,16,8) rbc= rb[0]*256 + rb[1] rbc2= self.twos_comp(rbc,16) return rbc2 def twos_comp(self,val, bits): # two's complement of value in bits if val&(1<<(bits-1)) != 0: val = val - (1<<bits) return val def check_spi_rd(self): #Readback Device ID to check the SPI Read self.get_prod_id() rb=self.get_prod_id() print ("--------------") print ("product_id readback:%s"%(rb)) if (rb == 3021) : print ("spi Read OK, Find DUT=ADcmXL3021") else: print ("spi Read Failure, Please check SPI timing and hardware connections") def software_reset(self): self.spi_read(self.GLOB_CMD) rb=self.spi_read(self.GLOB_CMD) rb=rb | 0x80 self.spi_write_word(self.GLOB_CMD,rb) #wait s time.sleep(0.5) def get_diag_sts(self): self.spi_read(self.DIAG_STS) rb=self.spi_read(self.DIAG_STS) return hex(rb) def get_temp_out(self): #return unit:C #self.set_page_id(page_id=0) self.spi_read(self.TEMP_OUT) rb=self.spi_read(self.TEMP_OUT) return (self.twos_comp(rb,16)*(-0.46)+460) def get_prod_id(self): #self.set_page_id(page_id=0) self.spi_read(self.PROD_ID) rb=self.spi_read(self.PROD_ID) return rb def set_user_scratch(self,user_scratch): #self.set_page_id(page_id=0) self.spi_write_word(self.USER_SCRATCH,user_scratch) def get_user_scratch(self): #self.set_page_id(page_id=0) self.spi_read(self.USER_SCRATCH) rb=self.spi_read(self.USER_SCRATCH) return rb def get_year_mon_day_rev(self): #self.set_page_id(page_id=0) self.spi_read(self.YEAR_MON) year_mon=self.spi_read(self.YEAR_MON) self.spi_read(self.REV_DAY) rev_day=self.spi_read(self.REV_DAY) return year_mon, rev_day def set_page_id(self,page_id): self.spi_write_word(self.PAGE_ID,page_id) def get_page_id(self): self.spi_read(self.PAGE_ID) rb=self.spi_read(self.PAGE_ID) return rb # MTC mode Register Settings: # AVG_CNT: decimation filter D after ADC fs=220ksps # FILT_CTL: FIR filter 32 taps # REC_CTRL: [bit1:0] Record mode control = 0b10 (MTC) # [bit13:12] Window Setting =01 (hanning default) # [bit11:8] SR settings =0b0001 (sr0 enabled, sr1~3 disabled) # GLOB_CMD: Bit11= record start/stop or external trigger # /BUSY signal will toggle when the data record USER_SCRATCHis stored and the alarms are checked. # 4096 DATA will be stored in X/Y/Z_BUF def mtc_set(self): self.spi_write_word(self.AVG_CNT,0x7421) self.spi_write_word(self.FILT_CTRL,0x0000) self.spi_write_word(self.REC_CTRL,0x1102) self.record_start() time.sleep(2) def mtc_read(self): gain=-0.001907 self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read2s(self.X_BUF) x=self.spi_read2s(self.X_BUF)*gain print (x) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read2s(self.Y_BUF) y=self.spi_read2s(self.Y_BUF)*gain print (y) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read2s(self.Z_BUF) z=self.spi_read2s(self.Z_BUF)*gain print (z) # MFFT mode Register Settings: # AVG_CNT: decimation filter D after ADC fs=220ksps # FILT_CTL: FIR filter 32 taps # REC_CTRL: [bit1:0] Record mode control = 0b00 (MFFT) # [bit13:12] Window Setting =01 (hanning default) # [bit11:8] SR settings =0b0001 (sr0 enabled, sr1~3 disabled) # FFT_AVG1: spectral average settings for sr0 and sr1, default (0x0108) # FFT_AVG2: spectral average settings for sr2 and sr3, default (0x0101) # GLOB_CMD: Bit11= record start/stop or external trigger # /BUSY signal will toggle when the data record USER_SCRATCHis stored and the alarms are checked. # 4096 DATA will be stored in X/Y/Z_BUF def mfft_set(self): self.spi_write_word(self.AVG_CNT,0x0000) self.spi_write_word(self.FILT_CTRL,0x0000) self.spi_write_word(self.REC_CTRL,0x1100) self.spi_write_word(self.FFT_AVG1,0x0108) self.spi_write_word(self.FFT_AVG2,0x0101) self.record_start() time.sleep(10) def mfft_read(self): self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read(self.X_BUF) x=self.spi_read(self.X_BUF) print (x) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read(self.Y_BUF) y=self.spi_read(self.Y_BUF) print (y) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read(self.Z_BUF) z=self.spi_read(self.Z_BUF) print (z) def get_avg_cnt(self): #self.set_page_id(page_id=0) self.spi_read(self.AVG_CNT) rb=self.spi_read_bytes(self.AVG_CNT) sr3=rb[0]>>4 sr2=rb[0]&0x0F sr1=rb[1]>>4 sr0=rb[1]&0x0F return [sr3,sr2,sr1,sr0] def set_buf_pntr(self,buf_pntr): #self.set_page_id(page_id=0) self.spi_write_word(self.BUF_PNTR,buf_pntr) def record_start(self): self.spi_read(self.GLOB_CMD) rb=self.spi_read(self.GLOB_CMD) rb=rb | 0x0800 self.spi_write_word(self.GLOB_CMD,rb) def self_test(self): self.spi_read(self.GLOB_CMD) rb=self.spi_read(self.GLOB_CMD) rb=rb | 0x0004 self.spi_write_word(self.GLOB_CMD,rb) time.sleep(1) rb=self.spi_read_bytes(self.DIAG_STAT) return rb if __name__ == "__main__": try: if 1: time.sleep(1) except KeyboardInterrupt: spi.close() sys.exit(0)
# adcmxl3021 Driver in Python # SPI Master is using Raspberry Pi # spidev is the Raspberry Pi spi communication library # Date: 2019.7.11 import sys import spidev import time SPI_MAX_SPEED =1953125 class adcmxl3021(): #Configuration Constant based on ADcmXL3021 datasheet PAGE_ID =0x00 TEMP_OUT =0x02 SUPPLY_OUT =0x04 FFT_AVG1 =0x06 FFT_AVG2 =0x08 BUF_PNTR =0x0A REC_PNTR =0x0C X_BUF =0x0E Y_BUF =0x10 Z_BUF =0x12 X_ANULL =0x14 Y_ANULL =0x16 Z_ANULL =0x18 REC_CTRL =0x1A REC_PRD =0x1E ALM_F_LOW =0x20 ALM_F_HIGH =0x22 ALM_X_MAG1 =0x24 ALM_Y_MAG1 =0x26 ALM_Z_MAG1 =0x28 ALM_X_MAG2 =0x2A ALM_Y_MAG2 =0x2C ALM_Z_MAG2 =0x2E ALM_PNTR =0x30 ALM_S_MAG =0x32 ALM_CTRL =0x34 DIO_CTRL =0x36 FILT_CTRL =0x38 AVG_CNT =0x3A DIAG_STAT =0x3C GLOB_CMD =0x3E ALM_X_STAT =0x40 ALM_Y_STAT =0x42 ALM_Z_STAT =0x44 ALM_X_PEAK =0x46 ALM_Y_PEAK =0x48 ALM_Z_PEAK =0x4A TIME_STAMP_L =0x4C TIME_STAMP_H =0x4E REV_DAY =0x52 YEAR_MON =0x54 PROD_ID =0x56 SERIAL_NUM =0x58 USER_SCRATCH =0x5A REC_FLASH_CNT =0x5C MISC_CTRL =0x64 REC_INFO1 =0x66 REC_INFO2 =0x68 REC_PNTR =0x6A ALM_X_FREQ =0x6C ALM_Y_FREQ =0x6E ALM_Z_FREQ =0x70 STAT_PNTR =0x72 X_STASTIC =0x74 Y_STASTIC =0x76 Z_STASTIC =0x78 FUND_FREQ =0x7A FLASH_CNT_L =0x7C FLASH_CNT_H =0x7E PAGE_ID =0x00 def __init__(self, device=0, ce_pin=0): """ device: the SPI device (often 0) ce_pin: pass 0 for CE0, 1 for CE1, etc. device and ce_pin map to device file /dev/spidev{device}.{ce_pin} """ self.spi_init(device, ce_pin) def spi_init(self,device,ce_pin): """ Using "pinout" command to check the raspberry spi definition. device: SPI0 (0), SPI1 (1) ce_pin: CE0 (0), CE1 (1) SPI0 definition CE0 : GPIO8 (0) PIN24 CE1 : GPIO7 (1) PIN26 MOSI: GPIO10 PIN19 MISO: GPIO9 PIN21 SCLK: GPIO11 PIN23 SPI1 definition CE0 : GPIO18 (0) PIN12 CE1 : GPIO17 (1) PIN11PAGE_ID CE2 : GPIO16 (2) PIN36 MOSI: GPIO20 PIN38 MISO: GPIO19 PIN35 SCLK: GPIO21 PIN40 """ # init spi for communication self.spi = spidev.SpiDev() self.spi.open(device, ce_pin) # (x,0) == CE0, (x,1) == CE1 # Set 4-line spi mode self.spi.threewire =False # Set spi msb first self.spi.lsbfirst =False # Set clock phase and polarity to default # SPI_CPOL=0, SPI_CPHA=0 self.spi.mode =3 # Set SPI CS Active Low self.spi.cshigh =False # Set SPI clock rate: 7.8125MHz, cdiv=32, fsclk=250MHz/cdiv, cdiv = [2,4,8,16,32,...32768] self.spi.max_speed_hz=SPI_MAX_SPEED self.spi.bits_per_word =8 def spi_write(self, address, value): # Write value (1 byte) to address # Send instruction (command bit7=1 for write), address[6:0], and value address=address+0x80 self.spi.xfer([address, value]) def spi_write_word(self,address,value_16b): value_l=value_16b & 0xFF value_h=value_16b>>8 self.spi_write(address,value_l) self.spi_write(address+1,value_h) def spi_read_bytes(self, address): # Read # Send instruction (command bit7=0 for read), address bit6:0 rb=self.spi.xfer([address,0],SPI_MAX_SPEED,16,8) return rb def spi_read(self, address): # Read # Send instruction (command bit7=0 for read), address bit6:0 rb=self.spi.xfer([address,0],SPI_MAX_SPEED,16,8) rbc= rb[0]*256 + rb[1] return rbc def spi_read2s(self, address): # Read # Send instruction (command bit7=0 for read), address bit6:0 rb=self.spi.xfer([address,0],SPI_MAX_SPEED,16,8) rbc= rb[0]*256 + rb[1] rbc2= self.twos_comp(rbc,16) return rbc2 def twos_comp(self,val, bits): # two's complement of value in bits if val&(1<<(bits-1)) != 0: val = val - (1<<bits) return val def check_spi_rd(self): #Readback Device ID to check the SPI Read self.get_prod_id() rb=self.get_prod_id() print ("--------------") print ("product_id readback:%s"%(rb)) if (rb == 3021) : print ("spi Read OK, Find DUT=ADcmXL3021") else: print ("spi Read Failure, Please check SPI timing and hardware connections") def software_reset(self): self.spi_read(self.GLOB_CMD) rb=self.spi_read(self.GLOB_CMD) rb=rb | 0x80 self.spi_write_word(self.GLOB_CMD,rb) #wait s time.sleep(0.5) def get_diag_sts(self): self.spi_read(self.DIAG_STS) rb=self.spi_read(self.DIAG_STS) return hex(rb) def get_temp_out(self): #return unit:C #self.set_page_id(page_id=0) self.spi_read(self.TEMP_OUT) rb=self.spi_read(self.TEMP_OUT) return (self.twos_comp(rb,16)*(-0.46)+460) def get_prod_id(self): #self.set_page_id(page_id=0) self.spi_read(self.PROD_ID) rb=self.spi_read(self.PROD_ID) return rb def set_user_scratch(self,user_scratch): #self.set_page_id(page_id=0) self.spi_write_word(self.USER_SCRATCH,user_scratch) def get_user_scratch(self): #self.set_page_id(page_id=0) self.spi_read(self.USER_SCRATCH) rb=self.spi_read(self.USER_SCRATCH) return rb def get_year_mon_day_rev(self): #self.set_page_id(page_id=0) self.spi_read(self.YEAR_MON) year_mon=self.spi_read(self.YEAR_MON) self.spi_read(self.REV_DAY) rev_day=self.spi_read(self.REV_DAY) return year_mon, rev_day def set_page_id(self,page_id): self.spi_write_word(self.PAGE_ID,page_id) def get_page_id(self): self.spi_read(self.PAGE_ID) rb=self.spi_read(self.PAGE_ID) return rb # MTC mode Register Settings: # AVG_CNT: decimation filter D after ADC fs=220ksps # FILT_CTL: FIR filter 32 taps # REC_CTRL: [bit1:0] Record mode control = 0b10 (MTC) # [bit13:12] Window Setting =01 (hanning default) # [bit11:8] SR settings =0b0001 (sr0 enabled, sr1~3 disabled) # GLOB_CMD: Bit11= record start/stop or external trigger # /BUSY signal will toggle when the data record USER_SCRATCHis stored and the alarms are checked. # 4096 DATA will be stored in X/Y/Z_BUF def mtc_set(self): self.spi_write_word(self.AVG_CNT,0x7421) self.spi_write_word(self.FILT_CTRL,0x0000) self.spi_write_word(self.REC_CTRL,0x1102) self.record_start() time.sleep(2) def mtc_read(self): gain=-0.001907 self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read2s(self.X_BUF) x=self.spi_read2s(self.X_BUF)*gain print (x) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read2s(self.Y_BUF) y=self.spi_read2s(self.Y_BUF)*gain print (y) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read2s(self.Z_BUF) z=self.spi_read2s(self.Z_BUF)*gain print (z) # MFFT mode Register Settings: # AVG_CNT: decimation filter D after ADC fs=220ksps # FILT_CTL: FIR filter 32 taps # REC_CTRL: [bit1:0] Record mode control = 0b00 (MFFT) # [bit13:12] Window Setting =01 (hanning default) # [bit11:8] SR settings =0b0001 (sr0 enabled, sr1~3 disabled) # FFT_AVG1: spectral average settings for sr0 and sr1, default (0x0108) # FFT_AVG2: spectral average settings for sr2 and sr3, default (0x0101) # GLOB_CMD: Bit11= record start/stop or external trigger # /BUSY signal will toggle when the data record USER_SCRATCHis stored and the alarms are checked. # 4096 DATA will be stored in X/Y/Z_BUF def mfft_set(self): self.spi_write_word(self.AVG_CNT,0x0000) self.spi_write_word(self.FILT_CTRL,0x0000) self.spi_write_word(self.REC_CTRL,0x1100) self.spi_write_word(self.FFT_AVG1,0x0108) self.spi_write_word(self.FFT_AVG2,0x0101) self.record_start() time.sleep(10) def mfft_read(self): self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read(self.X_BUF) x=self.spi_read(self.X_BUF) print (x) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read(self.Y_BUF) y=self.spi_read(self.Y_BUF) print (y) self.set_buf_pntr(buf_pntr=0) for i in range(10): if i==0: self.spi_read(self.Z_BUF) z=self.spi_read(self.Z_BUF) print (z) def get_avg_cnt(self): #self.set_page_id(page_id=0) self.spi_read(self.AVG_CNT) rb=self.spi_read_bytes(self.AVG_CNT) sr3=rb[0]>>4 sr2=rb[0]&0x0F sr1=rb[1]>>4 sr0=rb[1]&0x0F return [sr3,sr2,sr1,sr0] def set_buf_pntr(self,buf_pntr): #self.set_page_id(page_id=0) self.spi_write_word(self.BUF_PNTR,buf_pntr) def record_start(self): self.spi_read(self.GLOB_CMD) rb=self.spi_read(self.GLOB_CMD) rb=rb | 0x0800 self.spi_write_word(self.GLOB_CMD,rb) def self_test(self): self.spi_read(self.GLOB_CMD) rb=self.spi_read(self.GLOB_CMD) rb=rb | 0x0004 self.spi_write_word(self.GLOB_CMD,rb) time.sleep(1) rb=self.spi_read_bytes(self.DIAG_STAT) return rb if __name__ == "__main__": try: if 1: time.sleep(1) except KeyboardInterrupt: spi.close() sys.exit(0)
I'm looking for a routine for the adcmxl3201 program