Post Go back to editing

ADXL355震动后测试数据错误问题

1.我测量的是钻孔倾角,1G测量范围,但工作过程中有很大的震动,在钻孔钻进过程中震动很大,可能有30G,但测量是静止状态测量。在测量过程中发现在井下测量数据时常不对,但关机后在地面测量又正常。

2.测量过程发现有时测量数据正常,有时错误,在震动中测量数据错误,在静止状态下也继续数据错误,有时静止状态数据却正常,我设置的测量范围是+-2G

3.如何解决在震动中测量错误,在静止状态测量能正确的问题?加速度每次开机上电都自动复位吗?我每次采样前复位一次能彻底解决测量数据错误问题吗?

4.如果需要用滤波器解决,滤波器如何设置,程序指令是什么?参数多少合适,我是静止状态下测量的,我设置滤波器输出是错误的。

5.在电路设计上有办法解决抗震问题吗?

6、我设置2G测量范围和4G测量范围测量静止状态下加速度值是一样的,正常吗?是否4G测量范围要小一半才对。

  • 1~5. 在强震动环境中,对加速度量程为+/-2g的设置来说,当加速度超过8g,过量程保护会被触发,加速度计输出接近0,也就是说这时候引入了非线性,后面的滤波器也解决不了。建议使用更大量程的ADXL357。6. 2G量程和4G量程读数不应该一样,应该4G量程小一半才对。