Post Go back to editing

MEMS 加速度计ADXL345的驱动代码

MEMS加速度计ADXL345是一款小而薄的低功耗3轴加速度计,分辨率高(13位),测量范围达±16g。数字输出数据为16位二进制补码格式,可通过SPI(3线或4线)或I2C数字接口访问,非常适合移动设备应用。它可以在倾斜检测应用中测量静态重力加速度,还可以测量运动或冲击导致的动态加速度。其高分辨率(4 mg/LSB),能够测量不到1.0°的倾斜角度变化。

ADXL345可以提供多种特殊检测功能。活动和非活动检测功能检测有无运动发生,以及任意轴上的加速度是否超过用户设置的限值。敲击检测功能可以检测单击和双击动作。自由落体检测功能可以检测器件是否正在掉落。这些功能可以映射到两个中断输出引脚中的一个。

产品详情可点击:http://www.analog.com/cn/products/mems/accelerometers/adxl345.html#product-overview  进行查看。

今天斑竹主要介绍下"ADXL345 驱动代码",这里主要涉及到ADXL345 驱动代码方面的内容,对于ADXL345 驱动代码感兴趣的大侠可以参考一下。

#include "adxl345.h"
#include "sys.h"
#include "delay.h"
#include "math.h"  
////////////////////////////////////////////////////////////////////////////////// 
//ALIENTEK战舰STM32开发板  
////////////////////////////////////////////////////////////////////////////////////初始化ADXL345.
//返回值:0,初始化成功;1,初始化失败.
u8 ADXL345_Init(void)
{     
IIC_Init();       //初始化IIC总线
if(ADXL345_RD_Reg(DEVICE_ID)==0XE5) //读取器件ID
{ 
  ADXL345_WR_Reg(DATA_FORMAT,0X2B); //低电平中断输出,13位全分辨率,输出数据右对齐,16g量程
  ADXL345_WR_Reg(BW_RATE,0x0A);  //数据输出速度为100Hz
  ADXL345_WR_Reg(POWER_CTL,0x28);     //链接使能,测量模式
  ADXL345_WR_Reg(INT_ENABLE,0x00); //不使用中断  
   ADXL345_WR_Reg(OFSX,0x00);
  ADXL345_WR_Reg(OFSY,0x00);
  ADXL345_WR_Reg(OFSZ,0x00);
  return 0;
}  
return 1;             
}  
//写ADXL345寄存器
//addr:寄存器地址
//val:要写入的值
//返回值:无
void ADXL345_WR_Reg(u8 addr,u8 val)
{
IIC_Start();      
IIC_Send_Byte(ADXL_WRITE);      //发送写器件指令 
IIC_Wait_Ack();   
    IIC_Send_Byte(addr);      //发送寄存器地址
IIC_Wait_Ack();                   
IIC_Send_Byte(val);       //发送值       
IIC_Wait_Ack();           
    IIC_Stop();      //产生一个停止条件    
}
//读ADXL345寄存器
//addr:寄存器地址
//返回值:读到的值
u8 ADXL345_RD_Reg(u8 addr)  
{
u8 temp=0;  
IIC_Start();      
IIC_Send_Byte(ADXL_WRITE); //发送写器件指令 
temp=IIC_Wait_Ack();   
    IIC_Send_Byte(addr);     //发送寄存器地址
temp=IIC_Wait_Ack();                   
IIC_Start();          //重新启动
IIC_Send_Byte(ADXL_READ); //发送读器件指令 
temp=IIC_Wait_Ack();   
    temp=IIC_Read_Byte(0);  //读取一个字节,不继续再读,发送NAK         
    IIC_Stop();     //产生一个停止条件     
return temp;    //返回读到的值
} 
//读取ADXL的平均值
//x,y,z:读取10次后取平均值
void ADXL345_RD_Avval(short *x,short *y,short *z)
{
short tx=0,ty=0,tz=0;   
u8 i; 
for(i=0;i<10;i++)
{
  ADXL345_RD_XYZ(x,y,z);
  delay_ms(10);
  tx+=(short)*x;
  ty+=(short)*y;
  tz+=(short)*z;   
}
*x=tx/10;
*y=ty/10;
*z=tz/10;
}
//自动校准
//xval,yval,zval:x,y,z轴的校准值
void ADXL345_AUTO_Adjust(char *xval,char *yval,char *zval)
{
short tx,ty,tz;
u8 i;
short offx=0,offy=0,offz=0;
ADXL345_WR_Reg(POWER_CTL,0x00);     //先进入休眠模式.
delay_ms(100);
ADXL345_WR_Reg(DATA_FORMAT,0X2B); //低电平中断输出,13位全分辨率,输出数据右对齐,16g量程
ADXL345_WR_Reg(BW_RATE,0x0A);  //数据输出速度为100Hz
ADXL345_WR_Reg(POWER_CTL,0x28);     //链接使能,测量模式
ADXL345_WR_Reg(INT_ENABLE,0x00); //不使用中断   ADXL345_WR_Reg(OFSX,0x00);
ADXL345_WR_Reg(OFSY,0x00);
ADXL345_WR_Reg(OFSZ,0x00);
delay_ms(12);
for(i=0;i<10;i++)
{
  ADXL345_RD_Avval(&tx,&ty,&tz);
  offx+=tx;
  offy+=ty;
  offz+=tz;
}   
offx/=10;
offy/=10;
offz/=10;
*xval=-offx/4;
*yval=-offy/4;
*zval=-(offz-256)/4;  
  ADXL345_WR_Reg(OFSX,*xval);
ADXL345_WR_Reg(OFSY,*yval);
ADXL345_WR_Reg(OFSZ,*zval);
}
//读取3个轴的数据
//x,y,z:读取到的数据
void ADXL345_RD_XYZ(short *x,short *y,short *z)
{
u8 buf[6];
u8 i;
IIC_Start();      
IIC_Send_Byte(ADXL_WRITE); //发送写器件指令 
IIC_Wait_Ack();   
    IIC_Send_Byte(0x32);     //发送寄存器地址(数据缓存的起始地址为0X32)
IIC_Wait_Ack();                   

  IIC_Start();          //重新启动
IIC_Send_Byte(ADXL_READ); //发送读器件指令
IIC_Wait_Ack();
for(i=0;i<6;i++)
{
  if(i==5)buf[i]=IIC_Read_Byte(0);//读取一个字节,不继续再读,发送NACK 
  else buf[i]=IIC_Read_Byte(1); //读取一个字节,继续读,发送ACK
  }            
    IIC_Stop();     //产生一个停止条件
*x=(short)(((u16)buf[1]<<8)+buf[0]);     
*y=(short)(((u16)buf[3]<<8)+buf[2]);     
*z=(short)(((u16)buf[5]<<8)+buf[4]);    
}
//读取ADXL345的数据times次,再取平均
//x,y,z:读到的数据
//times:读取多少次
void ADXL345_Read_Average(short *x,short *y,short *z,u8 times)
{
u8 i;
short tx,ty,tz;
*x=0;
*y=0;
*z=0;
if(times)//读取次数不为0
{
  for(i=0;i<times;i++)//连续读取times次
  {
   ADXL345_RD_XYZ(&tx,&ty,&tz);
   *x+=tx;
   *y+=ty;
   *z+=tz;
   delay_ms(5);
  }
  *x/=times;
  *y/=times;
  *z/=times;
}
}
//得到角度
//x,y,z:x,y,z方向的重力加速度分量(不需要单位,直接数值即可)
//dir:要获得的角度.0,与Z轴的角度;1,与X轴的角度;2,与Y轴的角度.
//返回值:角度值.单位0.1°.
short ADXL345_Get_Angle(float x,float y,float z,u8 dir)
{
float temp;
  float res=0;
switch(dir)
{
  case 0://与自然Z轴的角度
    temp=sqrt((x*x+y*y))/z;
    res=atan(temp);
    break;
  case 1://与自然X轴的角度
    temp=x/sqrt((y*y+z*z));
    res=atan(temp);
    break;
   case 2://与自然Y轴的角度
    temp=y/sqrt((x*x+z*z));
    res=atan(temp);
    break;
  }
return res*1800/3.14;
}
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.