问答
讨论
文档
Members
Tags
Cancel
常见问题
马上提问
Open Questions. Can you
help
?
adxl367 产生中断后,主mcu读取完毕传感器数据,adxl367的status 寄存器 的DATA_READY bit不置0
Not Answered
7 days ago
fail to read CHIPID ?
Not Answered
4 months ago
该专区内容有关MEMS专区的讨论和常见问题解答。 发帖前请阅读 Analog Devices EngineerZone 行为准则。
All Threads
by
GuangGuangde
MEMS专区
Latest
7 days ago
by
ADIYX
230
1
0
Not Answered
adxl367 产生中断后,主mcu读取完毕传感器数据,adxl367的status 寄存器 的DATA_READY bit不置0
0
Not Answered
主mcu通过i2c接口与adxl367通信,通信数据为400k 上电后处理流程如下: 1、配置复位寄存器 reg_soft_reset=0x1F,value=0x52 2、读取芯片信息 reg_devid_ad=0x00,value=0xAD reg_devid_mst=0x01,value=0x1D reg_parid=0x02,value=0xF7 reg_revid=0x03,vale=0x03 3、配置功能寄存器 reg_filter_ctl=0x2C,value=0x00 (Range...
accelerometers
Sensors and MEMS
ADXL367
230
1
0
by
AID
MEMS专区
Latest
7 days ago
by
ADIYX
187
1
0
Suggested Answer
datasheet
0
Suggested Answer
这个描述的意思是 X轴数据 高位只用了4bit,低位也只用了4bit的意思吗?但是为啥说是12位?
Datasheet/Specs
accelerometers
Sensors and MEMS
ADXL382
187
1
0
by
AlanYu
MEMS专区
Latest
1 month ago
by
ADIYX
311
1
0
Answered
ADXL357,Y轴出现异常;
0
Answered
ADXL357测量Z、Y两个方向的振动加速度,STM32通过SPI读取后,再通过DAC输出两个通道值:0g时输出5V,+0.5g输出10V,-0.5g输出0V; ①0g加速度时,通道Z输出正常,DAC保持输出5V±0.001V。通道Y输出异常,DAC电压从 5V±0.001V 缓慢下降至4.95V后,再恢复到5V,见下图; ②上图中加了高通,纵轴换算成了加速度g,也就是缓慢负向变动了约50mg; ③出现上述异常的概率较低,不容易复现。硬件上,两个通道的处理方式一模一样; ④STM32主控...
adxl357
hardware
异常
accelerometers
adxl355
Sensors and MEMS
dac
通道
Show More
311
1
0
by
fate42
MEMS专区
Latest
1 month ago
by
ADIYX
252
1
0
Answered
ADXL345的内部滤波器的衰减曲线是什么样的
0
Answered
当设置ODR=3200HZ,用做检测±1g的振动G值,从振动频率只有400HZ时测量值就开始衰减是符合滤波的衰减曲线的吗
hardware
accelerometers
Sensors and MEMS
adxl345
252
1
0
by
JimHuang
MEMS专区
Latest
2 months ago
by
JimHuang
371
2
0
Answered
Could you please tell me if there is a driver for the AD7768 in the Zephyr system?
0
Answered
Is there a driver for the AD7768 for the Zephyr system? Or is there a plan to develop a driver for the AD7768 on the Zephyr platform? Zephyr is a relatively new operating system for embedded systems, somewhat similar to Linux. Currently, the AD7768 project...
Analog to Digital Converters (ADCs)
ad7768
371
2
0
by
BJWL
MEMS专区
Latest
4 months ago
by
BJWL
504
2
0
Not Answered
fail to read CHIPID ?
0
Not Answered
Hi, Dear Sir, I just begin to touch AD5940 on the CN0565 Board, power connecting lik this : wish to read the CHIPID with spi2 using the code below: void AD5940_Initialize(void) { int i; /* Write following registers with its data sequentially whenever...
hardware
spi
sensors
Sensors and MEMS
AD5940 on CN0565 Board
ad5940
Electrochemical Sensors
Show More
504
2
0
by
hbzzm
MEMS专区
Latest
6 months ago
by
ADIYX
537
1
0
Answered
adxl1002 输出波动问题
0
Answered
ADXL1002 设计图: 使用示波器测量 R2 电阻输出端的模拟信号,在静止不动的状态下,输出的波动超过了25mv(1g),峰峰值有80mv,这可能是什么原因造成的?
sensors
accelerometers
Sensors and MEMS
537
1
0
by
ADxl
MEMS专区
Latest
6 months ago
by
ADIYX
324
1
0
Answered
ADXL355自检
0
Answered
请问我自检输出0.3g 0.2g 1.26g ,差值不在区间这是什么原因
324
1
0
by
sicliyulu
MEMS专区
Latest
6 months ago
by
otway
2033
3
0
Answered
ADXL355 如何进行温度校准
+1
Answered
设备工作地点在高纬度地区。冬夏两季温差较大,是否有温度矫正方法?最大温差在 -20摄氏度到20摄氏度之间。
sensors
accelerometers
adxl355
Sensors and MEMS
2033
3
0
by
frankGosick55
MEMS专区
Latest
7 months ago
by
zhangwuji
1968
9
0
Suggested Answer
adxl382的三轴数据交换
+1
Suggested Answer
问题现象 主要是发现在静止状态下,运行大概15分钟,在stream FIFO模式下,出现z轴数据移动到Y轴,(也有时候到x轴。) 判断方式 已经确认,从FIFO里读出的数据的channel id都是正确的,可以看到下图,0x01 为Y轴,而0x020F则是1G。 这个的结果数据是从FIFO直接确认的(看来keil调试,所以可以排除后面组包导致的问题) 初始化逻辑 读取fifo按照 先读取fifo ready和对比watermark 最后去取数据...
ADXL382
1968
9
0
View All Threads
by
fate42
MEMS专区
Latest
1 month ago
by
ADIYX
252
1
0
Answered
ADXL345的内部滤波器的衰减曲线是什么样的
0
Answered
当设置ODR=3200HZ,用做检测±1g的振动G值,从振动频率只有400HZ时测量值就开始衰减是符合滤波的衰减曲线的吗
hardware
accelerometers
Sensors and MEMS
adxl345
252
1
0
by
AlanYu
MEMS专区
Latest
1 month ago
by
ADIYX
311
1
0
Answered
ADXL357,Y轴出现异常;
0
Answered
ADXL357测量Z、Y两个方向的振动加速度,STM32通过SPI读取后,再通过DAC输出两个通道值:0g时输出5V,+0.5g输出10V,-0.5g输出0V; ①0g加速度时,通道Z输出正常,DAC保持输出5V±0.001V。通道Y输出异常,DAC电压从 5V±0.001V 缓慢下降至4.95V后,再恢复到5V,见下图; ②上图中加了高通,纵轴换算成了加速度g,也就是缓慢负向变动了约50mg; ③出现上述异常的概率较低,不容易复现。硬件上,两个通道的处理方式一模一样; ④STM32主控...
adxl357
hardware
异常
accelerometers
adxl355
Sensors and MEMS
dac
通道
Show More
311
1
0
by
JimHuang
MEMS专区
Latest
2 months ago
by
JimHuang
371
2
0
Answered
Could you please tell me if there is a driver for the AD7768 in the Zephyr system?
0
Answered
Is there a driver for the AD7768 for the Zephyr system? Or is there a plan to develop a driver for the AD7768 on the Zephyr platform? Zephyr is a relatively new operating system for embedded systems, somewhat similar to Linux. Currently, the AD7768 project...
Analog to Digital Converters (ADCs)
ad7768
371
2
0
by
hbzzm
MEMS专区
Latest
6 months ago
by
ADIYX
537
1
0
Answered
adxl1002 输出波动问题
0
Answered
ADXL1002 设计图: 使用示波器测量 R2 电阻输出端的模拟信号,在静止不动的状态下,输出的波动超过了25mv(1g),峰峰值有80mv,这可能是什么原因造成的?
sensors
accelerometers
Sensors and MEMS
537
1
0
by
ADxl
MEMS专区
Latest
6 months ago
by
ADIYX
324
1
0
Answered
ADXL355自检
0
Answered
请问我自检输出0.3g 0.2g 1.26g ,差值不在区间这是什么原因
324
1
0
by
jike
MEMS专区
Latest
8 months ago
by
ADIYX
468
1
0
Answered
The adxl367 uses fifo, non-interruptible mode
0
Answered
My intended purpose is to read the latest 64*2 sets of three-axis data from the FIFO, as configured in my setup: I have configured the FIFO in stream mode, set the FIFO_SAMPLES register to 64, and set the ODR to 400Hz. Of course, I'm not using interrupts...
ADXL367 FIFO
sensors
accelerometers
Sensors and MEMS
468
1
0
by
jike
MEMS专区
Latest
8 months ago
by
jike
1411
5
0
Answered
The adxl367 uses fifo, non-interruptible mode, and is unable to obtain a specified number of data
+1
Answered
I use the FIFO of ADXL367 and set it to stream mode, hoping to save 64 sets of X, Y, and Z-axis data with a sampling frequency of 400Hz. I poll the FIFO data every 1 second (without using interrupts), but I always find 513 data entries when reading the...
ADXL367 FIFO
Datasheet/Specs
sensors
accelerometers
Sensors and MEMS
ADXL367
Show More
1411
5
0
by
jike
MEMS专区
Latest
8 months ago
by
jike
663
2
0
Answered
ADXL367设置FIFO采样长度后,使用轮询方式1s读取一次(非中断),但和预期的不一致
0
Answered
I use the FIFO of ADXL367 and set it to stream mode, hoping to save 64 sets of X, Y, and Z-axis data with a sampling frequency of 400Hz. I poll the FIFO data every 1 second (without using interrupts), but I always find 513 data entries when reading the...
Datasheet/Specs
sensors
accelerometers
Sensors and MEMS
ADXL367
Show More
663
2
0
by
muxiaoke
MEMS专区
Latest
9 months ago
by
ADIYX
661
3
0
Answered
adcmxl3021在rts模式下能不能长时间运行
0
Answered
adcmxl3021在rts模式下能不能长时间运行,我使用adcmxl3021在rts模式下运行一个小时以后,在使用传感器,读取的所有数据都是零是为什么
661
3
0
by
noway1
MEMS专区
Latest
10 months ago
by
ADIYX
612
1
0
Answered
adxl355读数异常,三轴中某一轴数据始终为0
0
Answered
adxl355芯片,我这边做了一批设备,一开始全部工作正常,后续有一次经拆装后,个别出现了三轴中某一轴读数全为0的情况,其余两轴读数正常(还有一个是xz轴异常,y轴正常,其余的为X轴异常,yz正常或z轴异常,xy正常),请问出现这种现象可能的原因是什么?拆装过程中过大的外部激励是否会导致这种现象,以及有什么解决方法?
hardware
sensors
accelerometers
adxl355
Sensors and MEMS
Show More
612
1
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More