在数据手册第29页列出了MAX14830内部的寄存器,MAX14830的所有串口采用同一个时钟源,所以对和时钟相关的寄存器CLKSource、PLLConfig寄存器,只需要通过UART0进行一次配置即可。其他的寄存器都是和串口相关,由于MAX14830内部有4个独立的串口,每个串口可以单独配置为不同模式,所以和串口相关的这些寄存器需要对每个串口都要配置,在SPI通讯模式下,在寄存器地址字节中有U1U0两位用来确定是对哪个串口进行操作;在IIC通讯模式下,采用不同的地址来表示不同的接口,关于IIC接口下各个串口的地址请参考数据手册中的table 12.